Skip to main content
dreamevil
Visitor II
June 24, 2013
Question

stm32f407 I2C error: ADDR bit not set after the 7-bit address is sent

  • June 24, 2013
  • 1 reply
  • 1099 views
Posted on June 24, 2013 at 05:11

Hello, guys

I'm working on a stm32f407 chip and I wanna implement the I2C communication with it. But I have encountered some problems.

The following describes my configuration about I2C:

Enable clock for GPIOB and I2C.

Remap I2C1 port to PB6, PB7

PB6, 7 are configured in AF mode, open-drain, 50MHz output speed.

I2C clock input is equal to APB1: 42MHz

I2C_InitStruct.I2C_Mode = I2C_Mode_I2C;

I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2;

I2C_InitStruct.I2C_OwnAddress1 = 0x0A;  //Master address

I2C_InitStruct.I2C_Ack = I2C_Ack_Enable; 

I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; //7 bit address mode

I2C_InitStruct.I2C_ClockSpeed = 100000; // speed = 300K

At last, the I2C peripheral is enabled.

After these configuration, I was able to generate a start condition, and the status register is right.

However, when I was trying to send the 7-bit slave address with bit0=0 (indicating a write operation according to EEPROM manual), the two status register value is 0x00070080. Only the BUSY, MSL, TRA,TxE bits are set. The ADDR bit is still keeping as 0.

I don't know why the ADDR keeps reset, when the status of AF and TxE is right. I think a rights status of AF and TxE means a successful sending of address. Then what's wrong with the ADDR bit?

Will anybody give me some advice about the possible reason for it? I have been stuck here for several days.

Thank you!

Wenlong Li

#stm32 #i2c #cm4 #addr-bit
This topic has been closed for replies.

1 reply

zzdz2
Associate
June 24, 2013
Posted on June 24, 2013 at 21:02

You can try to perform software I2C reset before configuring I2C.

I had somewhat similar problem with STM32F1 but it couldn't always generate start condition, sometimes it worked and sometimes not, weird.

Then I added software I2C reset and now it works flawlessly.