Skip to main content
Wood.Andy
Associate III
December 22, 2018
Question

STM32F407 - HSE Bypass using external clock.

Hi

I wish to use an external clock into PH0 from an oscillator module already present in my design.

Does this mean PH1 becomes a spare pin?

Thanks

Andy.

    This topic has been closed for replies.

    6 replies

    Uwe Bonnes
    Chief
    December 22, 2018

    HSEBYP needs HSEON and HSEON withh use PH0/1. I fear you can't use PH1 with external HSE. Perhaps try do some experiments . Perhaps PH1 is usable as Input pin.

    Wood.Andy
    Wood.AndyAuthor
    Associate III
    December 22, 2018

    Hi Uwe

    Will probably have to give it a try if I don't get a definite answer.

    Thanks

    Andy.

    waclawek.jan
    Super User
    December 23, 2018

    RM0090 clearly says:

    The external clock signal (square, sinus or triangle) with ~50% duty cycle has to drive the OSC_IN pin while the OSC_OUT pin should be left HI-Z.

    Also ch.8.3.14 Using the OSC_IN/OSC_OUT pins as GPIO PH0/PH1 port pins says that PH0/PH1's GPIO is overridden when HSEON is set.

    But of course an experiment is worth thousand words.

    JW

    PVand.9
    Associate
    December 17, 2020

    I have the same situation on a NucleoL053 where a 8MHz signal is supplied to the STM32L053 on the PH0 pin. The PH1_pin seems not to be controllable and stays Hi_Z.

    Tesla DeLorean
    Guru
    December 17, 2020

    STM32L072CZ PH1 not a GPIO w/BYPASS

    Ran into this with the Grashopper LoRa board, see this thread for context

    https://community.st.com/s/feed/0D50X00009bLS7uSAG

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..