Skip to main content
totti001
Associate III
January 19, 2015
Question

Stm32f407 hang up in system memory when debug

  • January 19, 2015
  • 0 replies
  • 486 views
Posted on January 19, 2015 at 20:00

Hello everybody!

I've a very strange error. I've running application for stm32f407. I can download the code and it's working well. But when I want to debug with CoIDE the code stopped at 1FFF39c4 so in the system memory. At this point I reset the debugger and the code stop at the main function. I don't know the problem.

Can anyobody help me?
    This topic has been closed for replies.