Question
STM32F407 FSMC synchronous burst AHB size?
Posted on April 30, 2013 at 11:02
Hi.
I have a problem with FMSC. I want to use FSMC single synchronous burst transfer with PSRAM. The memory has a 16bit data width and i read into ref. manual that ''When the selected bank is configured in synchronous burst mode, if an AHB single-bursttransaction is requested, the FSMC performs a burst transaction of length 1 (if the AHB
transfer is 16-bit), or length 2 (if the AHB transfer is 32-bit) and de-assert the chip select
signal when the last data is strobed.''.
Can I choose the AHB size or it is fixed to 32bit?
Best regards Przemek #stm32f4-fsmc-psram