Skip to main content
MDavo
Visitor II
May 15, 2019
Question

Stm32f407 damaged and overheat when SPI communication is running

  • May 15, 2019
  • 2 replies
  • 749 views

I'm using SPI Protocol in two STM32F407ZGT6 , one master and one slave

Board has 3.3v LDO regulator and Input Voltage has 5v

When power supply connected SPI program correctly work but in this case when disconnect SPI wires and connect again we face of overheating and ic damaged

I read about hot swapping ( replacing or adding components without stopping or shutting down the system ) in the web but can't find any resource in STM32 MCU

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 15, 2019

The techniques aren't exactly STM32 specific.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
May 15, 2019

"overheating and ic damaged" is normally a sign of pin voltages above maximum ratings. Review your schematic, wiring and setup/