Skip to main content
Associate
Apr 11, 2024 11:10 AM UTC
Question

STM32F405芯片USART 2M波特率下DMA收发丢数据

我用板子A:STM32H743VIT6,HAL库开发,版本v1.9.0

HSE=20M,主频480M

串口1使能,DMA发送,IDLE+DMA接收数据。

发送使用1ms定时器进行DMA串口发送,发送间隔1ms,发送数据长度18字节。

板子B:STM32F405RGT6,HAL库开发,版本v1.27.0

HSE=8M,主频168M

串口2使能,DMA发送,IDLE+DMA接收数据。

数据发送使用1ms定时器,10ms间隔通过DMA发送数据,发送数据长度18字节。

连线

板子A的Tx-板子B的Rx。

板子A的Rx-板子B的Tx。

问题:

H7板子数据发送正常,统计1s内,理论应发1000*18=18000字节,实际收到18000字节。

但是F4板子数据收到不足18000字节,发送数据也丢字节。

IDLE中断没有耗时操作,只把收到数据长度进行累加,然后退出。

 

This topic has been closed for replies.

3 replies

loganm122Author
Associate
Apr 11, 2024 11:13 AM UTC

使用UART,波特率2Mbps,1停止位,无校验,无流控

mƎALLEm
ST Technical Moderator
Apr 11, 2024 11:14 AM UTC

Hello,

In english please.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
loganm122Author
Associate
Apr 11, 2024 11:17 AM UTC

STM32F405 chip USART 2M baud DMA received and sent data lost
I use board A: STM32H743VIT6, HAL library development, version v1.9.0 HSE = 20M, main frequency 480M serial port 1 enabled, DMA send, IDLE + DMA receive data. Send using 1ms timer for DMA serial send, send interval 1ms, send data length 18 bytes. Board B: STM32F405RGT6, HAL library development, version v1.27.0 HSE = 8M, main frequency 168M serial port 2 enabled, DMA send, IDLE + DMA receive data. Data send using 1ms timer, 10ms interval through DMA send data, send data length 18 bytes. Connect board A's Tx - board B's Rx. Board A's Rx - board B's Tx. Problem: H7 board data send normal, statistics within 1s, the theory should send 1000*18 = 18000 bytes, the actual received 18000 bytes. But F4 board data received less than 18000 bytes, send data also lost bytes. IDLE interrupt without time-consuming operation, only the length of the data received accumulated, and then exit. I use board A: STM32H743VIT6, HAL library development, version v1.9.0 HSE = 20M, main frequency 480M serial port 1 enabled, DMA send, IDLE + DMA receive data. Send using 1ms timer for DMA serial send, send interval 1ms, send data length 18 bytes. Board B: STM32F405RGT6, HAL library development, version v1.27.0 HSE = 8M, main frequency 168M serial port 2 enabled, DMA send, IDLE + DMA receive data. Data send using 1ms timer, 10ms interval through DMA send data, send data length 18 bytes. Connect board A's Tx - board B's Rx. Rx of board A - Tx of board B. Problem: H7 board data transmission is normal, statistics within 1s, the theory should send 1000*18=18000 bytes, the actual received 18000 bytes. But F4 board data received less than 18000 bytes, the transmitted data also lost bytes. IDLE interrupt has no time-consuming operation, only accumulates the length of the received data, and then exits.