Skip to main content
liutaohappy2009
Visitor II
November 25, 2015
Question

stm32f405xx CAN Remote frame

  • November 25, 2015
  • 0 replies
  • 469 views
Posted on November 25, 2015 at 05:32

Hi ,

I'm using

a

STM32F405,my purpose is to receive the remote frame .but FIFO0 is not to receive the message . Namely , the function ''CAN2_RX0_IRQHandler'' interrupter is not access. 

My CONFIG is:

  hcan2.Init.Mode = CAN_MODE_NORMAL;

  hcan2.Init.SJW = CAN_SJW_1TQ;

  hcan2.Init.BS1 = CAN_BS1_3TQ;

  hcan2.Init.BS2 = CAN_BS2_2TQ;

  hcan2.Init.TTCM = DISABLE;

  hcan2.Init.ABOM = DISABLE;

  hcan2.Init.AWUM = DISABLE;

  hcan2.Init.NART = DISABLE;

  hcan2.Init.RFLM = DISABLE;

  hcan2.Init.TXFP = DISABLE;

My Filter setup is:

  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;

  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;

  sFilterConfig.FilterIdHigh = 0x0000;

  sFilterConfig.FilterIdLow = 0x0000;

  sFilterConfig.FilterMaskIdHigh = 0x0000;

  sFilterConfig.FilterMaskIdLow = 0x0000;

  sFilterConfig.FilterFIFOAssignment = 0;

  sFilterConfig.FilterActivation = ENABLE;

 Can someone help to solve the question ,thank you all.

#stm32-can-remote
This topic has been closed for replies.