Skip to main content
Associate III
October 18, 2023
Solved

STM32F405 - PWM complementary signals

  • October 18, 2023
  • 1 reply
  • 1366 views

Hello,

We are looking at using a STM32F405 in our power design LLC/PFC where we would need 4 complementary signals. 2 for the LLC and 2 for the PFC.

Looking at the reference manual I see the following:

17.3.11 Complementary outputs and dead-time insertion
The advanced-control timers (TIM1 and TIM8) can output two complementary signals and
manage the switching-off and the switching-on instants of the outputs.

So, it looks like for this part there is only the two complementary signals on TIM1 and TIM8?

Thanks for any insight.

Brent

 

 

This topic has been closed for replies.
Best answer by TDK

TIM1 and TIM8 each have 3 complimentary channels. CH4N isn't available on either.

They are on independent pins, so a total of 6 channels are available.

1 reply

TDK
TDKBest answer
October 18, 2023

TIM1 and TIM8 each have 3 complimentary channels. CH4N isn't available on either.

They are on independent pins, so a total of 6 channels are available.

"If you feel a post has answered your question, please click ""Accept as Solution""."