Skip to main content
aurelie
Visitor II
October 14, 2013
Question

STM32F405 - No clock on SPI

Posted on October 14, 2013 at 11:27

Hello,

I've some problems with the SPI interface of the STM32F405 microcontroller. I hope someone could help me.

I've a F-RAM connected to the STM32F405 via SPI. I'll checked pin connection and GPIO configuration with an oscilloscope ( set/reset IO), all works.

But I'm not able to receive or transmit data with SPI interface. There is no clock generating on the Clock pin (PC10).

To my code :

    GPIO_InitTypeDef GPIO_InitStructure;

    SPI_InitTypeDef  SPI_InitStructure;

    

    SPI_I2S_DeInit( SPI3);

    

        /* Enable GPIO and SPI Periph Clock */

    RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOA, ENABLE );

    RCC_APB1PeriphClockCmd( RCC_APB1Periph_SPI3, ENABLE );

    

    /* Connect CLK, MISO, MOSI and CS on AF6 */

    GPIO_PinAFConfig( GPIOC, GPIO_Pin_10, GPIO_AF_SPI3 );

    GPIO_PinAFConfig(

GPIOC

,

GPIO_Pin_11

, GPIO_AF_SPI3 );

    GPIO_PinAFConfig(

GPIOC

,

GPIO_Pin_12

, GPIO_AF_SPI3 );

    GPIO_PinAFConfig( GPIOA,

GPIO_Pin_4

, GPIO_AF_SPI3 );

    

    /* Configure SPI pins: ---------------------------------------------------*/

    /* Configure SCK MISO and MOSI pins as Alternate Function Push Pull */

    GPIO_InitStructure.GPIO_Pin   =

GPIO_Pin_10

|

GPIO_Pin_11

|

GPIO_Pin_12

;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode  = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_NOPULL;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

    GPIO_Init( GPIOC, &GPIO_InitStructure );

    

    /* Configure CS pin  */

    GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_4;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_Init( GPIOA, &GPIO_InitStructure ); 

    GPIO_SetBits( GPIOA,

GPIO_Pin_4

);

    

    /* Configure Write Protection pin (active low) */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_Init( GPIOB, &GPIO_InitStructure ); 

    GPIO_SetBits(

GPIOB

,

GPIO_Pin_0

);

    

    /* SPI Configuration -----------------------------------------------------*/

    SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

    SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

    SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;                             

    SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;                           

    SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;                               

    SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256;      

    SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

    SPI_Init( SPI3, &SPI_InitStructure ); 

    

    /* TEST */

     /* Enable the SPI peripheral */

    SPI_Cmd( SPI3, ENABLE );

    /* Enable CS (active low) */

     GPIO_ResetBits( GPIOA, GPIO_Pin_4);

    while( 1 )

    {

        SPI_I2S_SendData( SPI3, 0xAA );

    }

Thanks & Best regards,

Aurélie.
    This topic has been closed for replies.

    1 reply

    John F.
    Associate III
    October 14, 2013
    Posted on October 14, 2013 at 12:57

    void GPIO_PinAFConfig (GPIO_TypeDef *GPIOx, uint16_t GPIO_PinSource, uint8_t GPIO_AF)

    Function takes a GPIO_PinSource argument : specifies the pin for the Alternate function. This parameter can be GPIO_PinSourcex where x can be (0..15).