Skip to main content
Angelo1
Associate III
March 30, 2014
Question

stm32f405 malloc issue

Posted on March 31, 2014 at 01:11

Dear,

as in several examples, i implemented my _sbrk function to be able to use malloc, as (copied from examples):

extern int  _end;

/*

 * _sbrk needed for malloc

 */

caddr_t _sbrk ( int incr ) {

        static unsigned char *heap = NULL;

        unsigned char *prev_heap;

        if (heap == NULL) {

                heap = (unsigned char *)&_end;

        }

        prev_heap = heap;

        /* check removed to show basic approach */

        heap += incr;

        return (caddr_t) prev_heap;

}

Program compiles fine, no warnings, if i call directly _sbrk to allocate memory (instead of malloc) it works perfect, if i instead call ''malloc'', i see that _sbrk is called, but the return value of malloc is an null pointer (0).

Probably, malloc after calling sbrk do some other checks, and returns 0.

Every help is appreciated.

Thanks

#worst-forum-software-ever
    This topic has been closed for replies.

    13 replies

    Andrew Neil
    Super User
    March 31, 2014
    Posted on March 31, 2014 at 09:24

    This stuff is specific to the particular toolchain you're using - which you omitted to mention!

    What does your toolchain documentation say?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    March 31, 2014
    Posted on March 31, 2014 at 09:24

    (forum playing-up again)

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    chen
    Associate II
    March 31, 2014
    Posted on March 31, 2014 at 11:03

    Hi

    Would you happen to be using Atollic and FreeRTOS?

    When you called _sbrk() - was this before the scheduler started?

    When you called malloc() - was this after the scheduler started?

    Angelo1
    Angelo1Author
    Associate III
    March 31, 2014
    Posted on March 31, 2014 at 11:31

    Dear

    thanks,

    i am using

    /opt/gcc-arm-none-eabi-4_8-2013q4/bin/arm-none-eabi-gcc

    compile options are currently:

    OPTIMIZATION=-fdata-sections -ffunction-sections -fstrict-aliasing -O2 -mfpu=fpv4-sp-d16$

    CFLAGS  =-mthumb -mcpu=cortex-m4 -Wall $(OPTIMIZATION) -c -Iinclude -I$(INCSTM) -I$(INCC$

    ASFLAGS =-mthumb -mcpu=cortex-m4 -Wall $(OPTIMIZATION) -c -D__ASSEMBLY__

    LDFLAGS =-mthumb -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -nostartfiles -T stm$

    My guess is that ''malloc'' is doing some additional checks after calling _sbrk (maybe taking references from the linker file, i can attach it eventually), and returning 0.

    _sbrk is called from malloc since if i put a while(1) inside the program block.

    If i call the _sbrk function, it works perfect and returns a valid pointer.

    Many thanks

    Angelo1
    Angelo1Author
    Associate III
    March 31, 2014
    Posted on March 31, 2014 at 11:32

    Dear

    thanks,

    i am using

    /opt/gcc-arm-none-eabi-4_8-2013q4/bin/arm-none-eabi-gcc

    compile options are currently:

    OPTIMIZATION=-fdata-sections -ffunction-sections -fstrict-aliasing -O2 -mfpu=fpv4-sp-d16$

    CFLAGS  =-mthumb -mcpu=cortex-m4 -Wall $(OPTIMIZATION) -c -Iinclude -I$(INCSTM) -I$(INCC$

    ASFLAGS =-mthumb -mcpu=cortex-m4 -Wall $(OPTIMIZATION) -c -D__ASSEMBLY__

    LDFLAGS =-mthumb -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -nostartfiles -T stm$

    My guess is that ''malloc'' is doing some additional checks after calling _sbrk (maybe taking references from the linker file, i can attach it eventually), and returning 0.

    _sbrk is called from malloc since if i put a while(1) inside the function the program blocks.

    If i call the _sbrk function, it works perfect and returns a valid pointer.

    -- sory for double posting, i get an error from the web at first ''OK'' and i tried again --

    Many thanks

    chen
    Associate II
    March 31, 2014
    Posted on March 31, 2014 at 11:50

    Hi

    Just examined the code for _sbrk() in detail.

    Curious - Where does _end get assigned to?

    Does the heap grow upwards or downwards?

    What happens when it reaches end of memory?

    chen
    Associate II
    March 31, 2014
    Posted on March 31, 2014 at 13:18

    Hi

    ''My guess is that ''malloc'' is doing some additional checks after calling _sbrk (maybe taking references from the linker file, i can attach it eventually), and returning 0.''

    Yes. Depends on the particular implementation of  malloc()

    When I last looked at it - I found the linux implementation.

    It creates pools of used memory - linking them into linked lists, so that they can be got to by the free.

    The _sbrk() will be asked to get a larger size than was asked for in malloc().

    The larger size should be a multiple of power of 2 (ie 16, 32, 64 etc)

    The larger size is needed so that a linked list header can be applied and wraps the memory that was asked for.

    Must be failing somewhere in this routine.

    Angelo1
    Angelo1Author
    Associate III
    March 31, 2014
    Posted on March 31, 2014 at 13:21

    Hi chen,

    thanks,

    i just copied that _sbrk function i found in several places.

    that ''end'' is the end of the ebss and the start (in memory as lower address) of the space reserved of the heap. Yes, that ''end'' is a bit misleading wordings, but i kept them from linker files and _sbrk examples. So, once the pointer is returned , memory address (kn heap) is increased of the object amount / memory size.

    It works great if i call _sbrk directly. There is something with gcc, malloc, and final checks of malloc, that makes returning a ''0'' pointer.

    chen
    Associate II
    March 31, 2014
    Posted on March 31, 2014 at 13:55

    Hi

    malloc() from gcc will assume you are working in some kind of OS.

    I assumed that you were using Atollic and FreeRTOS BUT I see you are using raw gcc.

    I think you may be missing some OS functions which malloc() is calling.

    Atollic provides a file called syscalls.c which provided enough 'OS calls' for gcc to work.

    I think you will have to figure out what else is needed.

    chen
    Associate II
    March 31, 2014
    Posted on March 31, 2014 at 13:58

    Atollic provided these :

    /* Functions */

    void initialise_monitor_handles()

    int _getpid( void )

    int _kill( int pid, int sig )

    void _exit( int status )

    int _write( int file, char *ptr, int len )

    caddr_t _sbrk( int incr )

    int _close( int file )

    int _fstat( int file, struct stat *st )

    int _isatty( int file )

    int _lseek( int file, int ptr, int dir )

    int _read( int file, char *ptr, int len )

    int _open( char *path, int flags, ... )

    int _wait( int *status )

    int _unlink( char *name )

    int _times( struct tms *buf )

    int _stat( char *file, struct stat *st )

    int _link( char *old, char *new )

    int _fork( void )

    int _execve( char *name, char **argv, char **env )