Associate II
January 12, 2014
Question
STM32F405 (64 pin) device configuration question
- 4 replies
- 1119 views
Posted on January 13, 2014 at 00:03
Hi,
I'm new to the STM32 processors and I'm using the Microexplorer tool to figure out the pin and device assignment. Unfortunately it seems like it isn't possible to activate an additional timer, which I need to generate a clock which is fed back into the SPI2 and SPI3 clock inputs. The timer should also support DMA request generation. The devices I utilize are:USB: FS deviceUSART: USART1 & USART3 in async modeI2C: I2C1SPI1: Full dp master with NSSSPI2 & SPI3: Tx slave only unidirectionalTIM5: 4 x PWM output (using output-compare)TIM8, TIM12: PWM input (using capture-compare)ADC: ADC1_IN10 and ADC1_IN11 are used+ 3x GPIO output + 1x GPIO inputWhy is not possible to use TIM1 in output-compare mode on PA8 (TIM1_CH1)? Microexplorer tells me that there is a conflict OTG_FS, SPI1 and SPI2. Where does this conflict come from? Is it not possible to only use a single output pin (CH1) of the timer?I attached the Microexplorer configuration. It would be great if someone could explain why this device conflict occurs.Martin