Skip to main content
Associate II
May 30, 2024
Question

STM32F401RE Systick issues

Hello, I have an issue with my code where I have configured SysTick and it triggers on every clock cycle, but I dont know how to make things trigger inside the main while loop

 

#include "main.h"
#include "functions.h"
#include <stdbool.h>
#include <stdlib.h>

union InterruptFlag flag = { .bits_access.flag= 0,
							 .bits_access.direction=0,
							 .bits_access.debounce= 0,
							 .bits_access.press = 0}; // Initialize to 0


void EXTI15_10_IRQHandler(void){

 flag.bits_access.flag = !flag.bits_access.flag; // Set the flag to indicate button press event
 EXTI->PR |= (1<<13); // Clear PR to re-enable EXTI interrupt

};



#define MAX_DUTY 500
#define MIN_DUTY 0
#define DEBOUNCE_DELAY 500
volatile uint32_t duty_cycle;
volatile uint16_t incrementer = 1;

int main(void){

 TIM2_INIT();
 TIM3_INIT();
 Interrupt_Init();
 SysTick->CTRL = SysTick->CTRL | (1 << 0) | (1 << 1) | (1 << 2);
 SysTick->LOAD = (84000 - 1); // 100 millisecond
 while (1) {
	 //LED_PWM();
	 if(flag_check()==true){
		 incrementer=0;
	 }
 }
}

void SysTick_Handler(void)
{
	LED_PWM();
}

bool flag_check(){
	return flag.bits_access.flag;
}



void LED_PWM() {
 TIM2->CCR1 = duty_cycle;
 incrementer=1;
 if (duty_cycle >= MAX_DUTY) {
 flag.bits_access.direction = false; // Change direction to decrement
 } else if (duty_cycle <= MIN_DUTY) {
 flag.bits_access.direction = true; // Change direction to increment
 }

 if (flag.bits_access.direction) {
 duty_cycle += incrementer; // Increment
 } else {
 duty_cycle -= incrementer; // Decrement
 }
}

 

This topic has been closed for replies.

1 reply

Karl Yamashita
Principal
May 30, 2024

If you're just trying to blink an LED at a different rate based off the System tick, then look at this tutorial 

https://www.youtube.com/watch?v=o0qhmXR5LD0

 

You can keep the System tick at it's default 1 ms tick.

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source