Question
stm32f401re nucleo: PLL configuration
Posted on November 26, 2015 at 13:54
Hello everybody!
I'm trying to configure the main PLL to generate the max clock frequency (84 MHz on this board), and I'm using the HSI as PLL source.I made some test:- test1: HCLK=70 MHzM=16N=140P=2AHB_PR=1APB1_PR=2APB2_PR=1As soon as I set the PLL output as HCLK, the uC stops working.I mean:- no blinking led- random value on general purpose registerI made some test:- test2: HCLK=35 MHzM=16N=140P=2AHB_PR=2APB1_PR=2APB2_PR=1The uC works normally.I'm missing some configuration (i.e. ART?), or the problem is the HSI and his accuracy?Could someone help me to figure it out? Thanks!Regards