Skip to main content
Associate
September 3, 2023
Question

STM32F401RE

  • September 3, 2023
  • 1 reply
  • 1059 views

AREA mycode, CODE

  EXPORT __main

myclock EQU 0x40023830

myDmode EQU 0x40020000

myDout EQU 0x40020014

myPU_PD EQU 0x4002080C

myPC13I EQU 0x40020810

  ENTRY

__main PROC

  NOP

;------------------------------Port C Clock Enable

  LDR R1,=myclock

  LDR R5,[R1]

  MOV R2,#1

  LSL R2,#2

  ORR R5,R2

  STR R5,[R1]

;------------------------------PC13 Pull-Up Pull-Down

  LDR R1,=myPU_PD

  LDR R5,[R1]

  MOV R2,#1

  LSL R2,#26

  ORR R5,R2

  STR R5,[R1]

 

;---------------------------Clock uygulama PA5 LED, PC13 User Button 

  LDR R1,=myclock

  LDR R5,[R1]

  MOV R2,#1

  LSL R2,#0

  ORR R5,R2

  STR R5,[R1]

;----------------------------Çikis uclari seçimi PA5  

  LDR R1,=myDmode

  LDR R5,[R1]

  MOV R2,#0x1

  LSL R2,#10

  ORR R5,R2

  STR R5,[R1]

;------------------------------Read PC13 pin

Re_PC13 LDR R1,=myPC13I

     LDR R5,[R1]

  MOV R2,#0x2000

  AND R5,R2

  CMP R5,#0

  BEQ myRun

  B Re_PC13

;----------------------------Led On

myRun NOP

One2 LDR R1,=myDout

  LDR R5,[R1]

  ;MOV R2,#0xF

  MOV R2,#0x1

  ;LSL R2,#12

  LSL R2,#5

  ORR R5,R2

  STR R5,[R1]

;---------------------------- Gecikme

  LDR R6,=0XFFFFF

Two1 SUB R6,#1

  CMP R6,#0

  BEQ One1

  B Two1

;---------------------------- LED off

One1 LDR R1,=myDout

  LDR R5,[R1]

  LDR R2,=0xFFFFFFCF

  AND R5,R2

  STR R5,[R1] 

;---------------------------- Gecikme

  LDR R6,=0XFFFFF

Two2 SUB R6,#1

  CMP R6,#0

  BEQ Re_PC13

  B Two2

;----------------------------

  ENDP

  END

 

I have a STM32F401RE . I have PA4 pin Input and PC7 pin Output. I need help. I need PA4 offset and PC7 offset. Can you rewrite the program using the new inputs and outputs?

This topic has been closed for replies.

1 reply

Issamos
Lead III
September 3, 2023

Hello @CCV  

This is a modified version of your code:

AREA mycode, CODE

 

EXPORT __main

 

myclock EQU 0x40023830

myDmode EQU 0x40020000

myDout EQU 0x40020014

myPU_PD EQU 0x4002080C

myPC4I EQU 0x40020810 ; PA4 as Input

myPC7O EQU 0x40020C14 ; PC7 as Output

 

ENTRY

 

__main PROC

 

  NOP

 

;------------------------------Port C Clock Enable

 

  LDR R1,=myclock

 

  LDR R5,[R1]

 

  MOV R2,#1

 

  LSL R2,#2

 

  ORR R5,R2

 

  STR R5,[R1]

 

;------------------------------PC4 Pull-Up Pull-Down

 

  LDR R1,=myPU_PD

 

  LDR R5,[R1]

 

  MOV R2,#1

 

  LSL R2,#4  

 

  ORR R5,R2

 

  STR R5,[R1]

 

;---------------------------Clock uygulama PA5 LED, PC7 Output

 

  LDR R1,=myclock

 

  LDR R5,[R1]

 

  MOV R2,#1

 

  LSL R2,#0

 

  ORR R5,R2

 

  STR R5,[R1]

 

;----------------------------Çikis uclari seçimi PC7 (0100) 

 

  LDR R1,=myDmode

 

  LDR R5,[R1]

 

  MOV R2,#0x4  

 

  LSL R2,#28

 

  ORR R5,R2

 

  STR R5,[R1]

 

;------------------------------Read PA4 pin

 

Re_PA4 LDR R1,=myPC4I

 

     LDR R5,[R1]

 

  MOV R2,#0x10  

 

  AND R5,R2

 

  CMP R5,#0

 

  BEQ myRun

 

  B Re_PA4

 

;----------------------------Led On (PC7 High)

 

myRun LDR R1,=myDout

 

  LDR R5,[R1]

 

  MOV R2,#0x80  

 

  ORR R5,R2

 

  STR R5,[R1]

 

;---------------------------- Gecikme

 

  LDR R6,=0XFFFFF

 

Two1 SUB R6,#1

 

  CMP R6,#0

 

  BEQ One1

 

  B Two1

 

;---------------------------- LED off (PC7 Low)

 

One1 LDR R1,=myDout

 

  LDR R5,[R1]

 

  MOV R2,#0xFFFFFF7F  

 

  AND R5,R2

 

  STR R5,[R1]

 

;---------------------------- Gecikme

 

  LDR R6,=0XFFFFF

 

Two2 SUB R6,#1

 

  CMP R6,#0

 

  BEQ Re_PA4

 

  B Two2

 

  ENDP

 

  END

  Hope this is helpful. If your question is answered please check this answer as best answer to be diffused.

Best regards.

II

CCVAuthor
Associate
September 4, 2023

Sorry its doesnt work

 

Issamos
Lead III
September 4, 2023

Hello again

Then, you can open an exemple of code in C that do the same thing and then open the Disassembly View which is well described in this post. This view will give a transaction of the C code to assembly language. Then you can copie the assembly code and use it in your project .

 

Hope this is helpful. If your question is answered please check this answer as best answer to be diffused.

 

Best regards.

 

II