Question
STM32F401 RTC ALARMA wake up CPU from StandBy with 16 seconds error. Why?
I'm configuring RTC AlarmA to wake up CPU from StandBy. I'am expecting to CPU became back at specified time, but it event occurs up to 16 seconds later.
uint32_t time;
uint32_t date;
uint32_t subsec;
do {
time = LL_RTC_TIME_Get(RTC);
date = LL_RTC_DATE_Get(RTC);
subsec = LL_RTC_TIME_GetSubSecond(RTC);
} while (subsec != LL_RTC_TIME_GetSubSecond(RTC));
sec = __LL_RTC_CONVERT_BCD2BIN(__LL_RTC_GET_SECOND(time));
min = __LL_RTC_CONVERT_BCD2BIN(__LL_RTC_GET_MINUTE(time));
hour= __LL_RTC_CONVERT_BCD2BIN(__LL_RTC_GET_HOUR(time));
sec+=10; //
LL_RTC_DisableWriteProtection(RTC);
CLEAR_BIT(PWR->CSR, PWR_CSR_EWUP);
LL_RTC_ALMA_Disable(RTC);
do {} while (!LL_RTC_IsActiveFlag_ALRAW(RTC));
LL_RTC_ClearFlag_ALRA(RTC);
LL_RTC_ALMA_ConfigTime(RTC, LL_RTC_ALMA_TIME_FORMAT_AM, __LL_RTC_CONVERT_BIN2BCD(hour), __LL_RTC_CONVERT_BIN2BCD(min), __LL_RTC_CONVERT_BIN2BCD(sec));
LL_RTC_ALMA_SetMask(RTC, LL_RTC_ALMA_MASK_DATEWEEKDAY | LL_RTC_ALMA_MASK_HOURS | LL_RTC_ALMA_MASK_MINUTES);
LL_RTC_ALMA_SetSubSecondMask(RTC, 0);
LL_RTC_ALMA_Enable(RTC);
LL_RTC_EnableWriteProtection(RTC);
TRACE_INFO("RTC->ALRMAR: 0x%08X\r\n",RTC->ALRMAR);
/* Enable the wake up pin */
SET_BIT(PWR->CSR, PWR_CSR_EWUP);
SET_BIT(PWR->CR, PWR_CR_PDDS | PWR_CR_CWUF | PWR_CR_CSBF);
SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SLEEPDEEP_Msk));
__WFI();If set time to WakeUp for example 00:00:10 -> CPU will WakeUp at 00:00:26 and so on. Always up to 16 seconds later.
What I do wrong?