STM32F401 - HAL_UART_Receive() - Buggy?
Hi all,
I believe HAL_UART_Receive() is buggy.
Test case:
uint8_t data[2] = {0xAA, 0xBB};
HAL_UART_Receive
(&huart1, &data[0], 1, 100);You would expect data[0] to be the data received from the USART, and data[1] to be left alone as 1 is the specified size in bytes.
This is not the case.
HAL_UART_Receive() whacks data[1] as well (sets it to a value of 0).
Its quite clear why this happens looking at the source for
HAL_UART_Receive()...
HAL_StatusTypeDef HAL_UART_Receive(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size, uint32_t Timeout)
{ uint16_t* tmp;...... tmp = (uint16_t*) pData;......
*tmp = (uint16_t)(huart->Instance->DR & (uint16_t)0x00FFU);
......
}
Seems to be a pretty basic mistake?