Hi @LSL 罗 and welcome to the Community :),
I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.
Here is the translation of your post using Google translate:
In the STM32F401 series, do the ADC_IN16 channel and the ADC_IN18 channel share the same channel?
If I understand correctly, if you refer to the RM0368 and precisely Figure 38. Temperature sensor and VREFINT channel block diagram, you can conclude that you can output Vsense on both channel ADC1_IN16 and ADC1_IN18.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thank you
Kaouthar
To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.