Skip to main content
PHolt.1
Senior
Jun 22, 2026 1:12 PM UTC
Question

STM32F4: Worst-case latency timer to DMA?

I am using TIM8 to generate a PWM waveform (a /wr signal to an LCD ST7789 controller) and the timer triggers DMA2 to load the next byte onto the PD8-PD15 bus. The 1st byte has to be loaded “manually”.

It works, and the ARR CCR3 CCR4 values can be adjusted to get the desired overall period, and data setup and hold times.

At 84MHz APB2, I am using ARR=11 to get a 71ns cycle time. So this thing is running pretty fast. The timer resolution is 1/168MHz. The ST7789 can go down to 66ns.

The problem is that roughly once in a million writes, bad data is loaded. It shows up as wrong colour pixels. With extensive debugging, AFAICT, the bad data is not present in the source buffer. What I do see on a scope is very rare faint edges on the data, around the /wr +ve edge, on which the data setup/hold time is out of spec. Sometimes the data changes at the same time as the /wr +ve edge!

Using ARR=15 or higher, the problem goes away. But then I get too-slow transfers.

It looks like there is a very rare huge latency in the DMA transfer, so the data on the PD8-PD15 bus is still the previous value. The correct number of writes takes place however, as only the one pixel (2 bytes, 16 bit RGB) is corrupted. In fact you need a magnifying glass to see the “snow”, on a 240x320 LCD.

To some extent the minimum ARR value needed to remove the “snow” depends on what else is running. DMA1 is also in use, for feeding SPI3, under another RTOS task. Then ETH has its own DMA controller. So there is opportunity for bus contention.

The really funny thing is that the “snow” pixels pop up 3-5x, at roughly 3Hz (on a 20fps display redraw) and then vanish for a few secs, then repeat. In the same place. So whatever is causing this is somehow synchronous to what DMA2 is doing. DMA2 is not used for anything else but DMA1 is.

What is the worst-case latency, and is there anything I can do to improve it? There is a priority setting but it applies only within DMA2 channels. It looks like very rarely the latency might be tens of ns.

The code is below. Start transfer, and init is below that.

	// TIM8 + DMA hardware /WR. CPU is idle during each burst.
//
// PC8 is a GPIO output (idle high) on entry. Flip it to AF3 (TIM8_CH3) for
// the pixel burst, then back to GPIO output afterwards so the next column's
// address setup can bit-bang /WR.
//
// Stream the buffer in <=256-byte bursts (RCR is 8-bit). For each burst:
// prime byte 0 onto PD8-15 (pulse 0 latches it), point DMA at bytes 1..n-1,
// then start TIM8. The CC4 compare event loads each subsequent byte while
// /WR is high so it settles ~54ns before the next latch.
//
// TWO RACE FIXES for the rare wrong/short filled-rectangle line:
// 1. __DSB() after EACH prime write (inside the loop) forces byte 0 onto
// the bus before the timer can latch it - covers byte 0 of every
// <=256 chunk, including the 2nd+ chunks of a >256 transfer.
// 2. After the timer self-stops (CEN clear), WAIT for the DMA transfer-
// complete flag (TCIF7) BEFORE disabling the stream. The timer stopping
// and the DMA draining its last byte are SEPARATE events; tearing the
// stream down on CEN-clear alone can catch the DMA still draining ->
// a whole line comes out short or wrong. This closes that race.
//
// HANG SAFETY: every spin-wait below is bounded by a ~100k iteration guard
// so a missed timer-stop or a DMA that errors (TEIF7/DMEIF7/FEIF7 set, but
// TCIF7 never set) degrades to a dropped/short line instead of hanging the
// LCD task for ever. 100k iterations >> the worst-case 256-byte burst
// (~20us), so the guards never trip in normal operation. The TCIF7 wait
// also exits on any DMA error flag, not just on completion.
LCD_DC_GPIO_PORT->BSRR = LCD_DC_PIN; // DAT: D/C=1
lcd_cs(0);

// PC8 -> AF3 (TIM8_CH3): the timer drives /WR for the DMA burst.
GPIOC->MODER = (GPIOC->MODER & ~(3u << (8*2))) | (2u << (8*2)); // PC8 = AF

uint32_t off = 0;
while (off < size)
{
uint32_t n = size - off;
if (n > 256u) n = 256u;
const uint8_t *b = &outbuf[off];

// CC4 DMA request OFF while we set up.
TIM8->DIER &= ~TIM_DIER_CC4DE;

// Prime byte 0, then a data barrier so the store lands before the
// timer can latch it (covers byte 0 of THIS chunk).
*((volatile uint8_t *)(&GPIOD->ODR) + 1) = b[0];
__DSB();

// Arm DMA for bytes 1..n-1 (none if n==1). CC4 in period k loads byte k+1.
if (n > 1u)
{
uint32_t guard;
DMA2_Stream7->CR &= ~DMA_SxCR_EN;
guard = 100000u;
while ((DMA2_Stream7->CR & DMA_SxCR_EN) && --guard) { }
if (guard == 0u) g_lcd_par8_dma_timeout++;
DMA2->HIFCR = (DMA_HIFCR_CTCIF7 | DMA_HIFCR_CHTIF7 |
DMA_HIFCR_CTEIF7 | DMA_HIFCR_CDMEIF7 | DMA_HIFCR_CFEIF7);
DMA2_Stream7->M0AR = (uint32_t)&b[1];
DMA2_Stream7->NDTR = n - 1u;
DMA2_Stream7->CR |= DMA_SxCR_EN;
}

// Load RCR (n pulses) via UG with CC4DE OFF, then clear UIF/CC4IF.
TIM8->RCR = n - 1u;
TIM8->EGR = TIM_EGR_UG;
TIM8->SR = 0;

// Clear any stale CC4 flag FIRST, THEN enable CC4 DMA, then start.
// (Enabling CC4DE while CC4IF is still set from the previous burst's
// last period fires an immediate spurious DMA request -> the whole
// burst shifts by one byte -> a wrong-colour run on that row.)
TIM8->SR = 0;
if (n > 1u) TIM8->DIER |= TIM_DIER_CC4DE;
TIM8->CR1 |= TIM_CR1_CEN;

// Wait for OPM to self-stop the timer (bounded). This is the guard that
// also covers the n==1 case (single primed byte, no DMA armed): it
// ensures the one OPM pulse has latched before teardown / PC8 flip.

uint32_t guard = 100000u;
while ((TIM8->CR1 & TIM_CR1_CEN) && --guard) { }
if (guard == 0u) g_lcd_par8_dma_timeout++;

// THEN wait for the DMA to finish draining its last byte before tearing
// the stream down - otherwise the timer-stop vs DMA-drain race can
// truncate the line. Exit on completion OR any DMA error (so an errored
// transfer, which never sets TCIF7, cannot hang here). Bounded by guard.
// (Skip if n==1: no DMA was armed.)
if (n > 1u)
{
uint32_t guard = 100000u;
while (!(DMA2->HISR & (DMA_HISR_TCIF7 | DMA_HISR_TEIF7 |
DMA_HISR_DMEIF7 | DMA_HISR_FEIF7)) && --guard) { }
if (guard == 0u) g_lcd_par8_dma_timeout++;
DMA2_Stream7->CR &= ~DMA_SxCR_EN;
}

TIM8->DIER &= ~TIM_DIER_CC4DE;

off += n;
}

// Very rarely the above PWM gen leaves /wr=0 so setting it to 1 below creates a +ve edge.
// Burst(s) done. OPM stops TIM8 at CNT=0, which is in the LOW half of the
// PWM mode-2 cycle, so CH3 leaves /WR (PC8, still in AF) driven LOW. If we
// flipped PC8 to GPIO-output-high here, the AF->GPIO handoff would drive
// /WR low->high while /CS is STILL LOW - a spurious rising edge, i.e. one
// extra pixel latched at the end of every burst (the end-of-transaction
// edges seen on the scope). So deselect FIRST: raise /CS while /WR is still
// (harmlessly) low, THEN bring /WR back to idle-high. The rising edge from
// the mode switch now happens with /CS already high and cannot latch.
lcd_cs(1); // /CS = 1 FIRST (deselect)

GPIOC->BSRR = WR_C_HIGH; // PC8 ODR = 1
__DSB(); // /WR-high store committed before PC8 leaves AF
GPIOC->MODER = (GPIOC->MODER & ~(3u << (8*2))) | (1u << (8*2)); // PC8 -> GPIO output (now follows ODR = high)
__DSB(); // ensure PC8 is GPIO before any following bit-bang
		/*
═══════════════════════════════════════════════════════════════════════════════
CC4-triggered DMA: load the next byte AFTER /WR has gone high, so it settles
during the high phase + next low phase and is rock-solid before the next latch.
═══════════════════════════════════════════════════════════════════════════════

PRINCIPLE
CH3 (CCR3) generates /WR via PWM mode 2: /WR low CNT 0..CCR3-1, high CNT CCR3..ARR.
Rising edge (the LATCH) is at CNT = CCR3.
CH4 (CCR4) is a DMA-TRIGGER ONLY channel (no output pin). Set CCR4 a few ticks
AFTER CCR3, so the CC4 event - and thus the DMA load of the next byte - happens
while /WR is already HIGH, a few cycles past the latch edge.
The byte loaded at CNT=CCR4 then has the rest of this period plus the next
period's low phase to settle before the NEXT rising edge at CNT=CCR3. No race.

CC-compare DMA requests are NOT gated by the repetition counter (unlike UPDATE),
so CC4 fires every period -> one byte per period, exactly what we want, while RCR
still bounds the burst length via OPM.

DMA MAPPING: TIM8_CH4 -> DMA2 Stream7, Channel 7.
(TIM8_UP was Stream1 Ch7; CC4 is a different stream. Stream7/Ch7 = TIM8_CH4/TRIG/COM.)

NOTE: PC8 is re-pointed to AF3 here via the raw AFR mux, but its MODER is left
as OUTPUT (set by HAL_GPIO_Init above). The DAT burst flips MODER to AF only
for the pixel stream and back, so the bit-bang init/address setup keep PC8 as
a GPIO output. The slew (OSPEEDR) set above carries over to the AF use.

A lot of time was spent on ARR CCR CCR4 values. There is a DMA trigger delay from
CCR4 to the DMA actually doing it, causing it to sometimes read what is probably the
same byte again, causing specs on the display. The probability is of the order of
1 in 100k. One needs to test with USB VCP and ETH all running. There is still
a little bit of snow with these settings but not readily visible.
*/

__HAL_RCC_TIM8_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();

// Pre-select AF3 for PC8 in the mux; leave MODER as OUTPUT (set above).
GPIOC->AFR[1] = (GPIOC->AFR[1] & ~(0xFu << ((WR_PIN_POS-8)*4)))
| (3u << ((WR_PIN_POS-8)*4)); // AF3

// Timer base
TIM8->PSC = 0;
TIM8->ARR = 11; // ARR=11 is 12 ticks ≈ 71ns (min ST7789 cycle is 66ns)
TIM8->RCR = 0; // set per-burst

TIM8->CR1 |= TIM_CR1_OPM; // one-pulse: self-stop after burst

// CH3 = /WR output, PWM mode 2 (low-first). Latch (rising edge) at CNT=CCR3.
TIM8->CCR3 = 8;
TIM8->CCMR2 &= ~TIM_CCMR2_OC3M;
TIM8->CCMR2 |= (7u << TIM_CCMR2_OC3M_Pos); // PWM mode 2
TIM8->CCMR2 |= TIM_CCMR2_OC3PE; // preload
TIM8->CCER |= TIM_CCER_CC3E; // CH3 output enable (drives PC8 in AF)
TIM8->BDTR |= TIM_BDTR_MOE; // main output enable

// CH4 = DMA-trigger only (no output pin). Compare at CCR4 generates the CC4
// event -> CC4 DMA request, loading the next byte while /WR is high.
TIM8->CCR4 = 9; // a few ticks after CCR3 (the latch)
TIM8->CCMR2 &= ~TIM_CCMR2_OC4M; // OC4M=0 (frozen) - still sets CC4IF on match
// (no CC4E - we don't need an output pin, just the compare event/flag)

// DMA requests from CC4 (NOT from update). UDE off; CC4DE on per-burst.
TIM8->DIER &= ~TIM_DIER_UDE;
// CC4DE toggled per-burst in LCD_Transmit_buf_DAT (kept off here).

// DMA2 Stream7 Ch7 = TIM8_CH4. byte->byte, mem-increment, mem->periph, PAR=ODR+1.
DMA2_Stream7->CR = 0;
while (DMA2_Stream7->CR & DMA_SxCR_EN) { }
DMA2_Stream7->PAR = (uint32_t)(&GPIOD->ODR) + 1u; // high byte -> PD8-15
DMA2_Stream7->CR =
(7u << DMA_SxCR_CHSEL_Pos) // channel 7 = TIM8_CH4
| (0u << DMA_SxCR_MSIZE_Pos) // memory size = byte
| (0u << DMA_SxCR_PSIZE_Pos) // periph size = byte
| DMA_SxCR_MINC // increment memory
| (1u << DMA_SxCR_DIR_Pos) // memory -> peripheral
| (2u << DMA_SxCR_PL_Pos); // priority high

TIM8->EGR = TIM_EGR_UG; // load shadow regs (timer idle)
GPIOC->BSRR = WR_C_HIGH; // PC8 = 1 (idle high), stays GPIO output

Start the transfer:

 

 

 

17 replies

PHolt.1
PHolt.1Author
Senior
Jul 2, 2026 10:19 PM UTC

I’ve checked the code; it seems right.

On the use of different RAM regions, it appears not possible on the 417.

On the 417: SRAM2 still contends with ETH buffer in SRAM1.

On the 437: the extra 64K bank (SRAM3) IS a separate bus-matrix slave. So on the 437, if you put the LCD buffer in that extra 64K bank (the top of the contiguous RAM) and if the ETH buffers stay in SRAM1/2, they WOULD be on separate slaves and wouldn't contend.

Does that sound right?

PHolt.1
PHolt.1Author
Senior
Jul 3, 2026 4:18 AM UTC

I tried placing the LCD buffer (the DMA source RAM) into the upper 64k of the 32F437 (SRAM3) and it makes no difference, so the contention must be happening elsewhere.

I did again confirm that an ETH burst size of 32 causes a bit of snow, whereas 1 does not.

 

LCE
Principal III
Jul 3, 2026 4:28 AM UTC

I have not checked all of the above code, maybe there’s also in the main loop too much going on and “blocking” the busses?

Do you use an OS or a state machine / self-made “task scheduler” in main?

PHolt.1
PHolt.1Author
Senior
Jul 3, 2026 7:09 AM UTC

FreeRTOS.

The basic project is several years old and very very solid. The LCD is a new add-on.

Basically, I have two ways to drive the LCD in parallel: bitbanged and DMA. The former runs fine (but uses up 100% CPU time, so not great for other tasks even though FR is pre-emptive) and the latter gets data corruption caused by a rare extreme latency from the timer to the DMA.

I can solve the problem by extending the (free running) timer cycle time to 15 cycles (15/168MHz). The ideal time would be 11 cycles, so 15 is costing me some speed, but I worked around it by optimising other stuff.

Other tasks doing “too much” and whatever interrupt load should not affect the timer->DMA process at all. It can of course affect bus loading and thus increase latency, but it amazes me that you can get so much latency on a DMA trigger. And very rare too. There is some strange mechanism involved.

I can also solve the snow by driving the LCD via SPI1, 42MHz is the max possible (APB2=84MHz) and that works clean but is half the speed of the parallel mode.

waclawek.jan
Super User
Jul 3, 2026 12:03 PM UTC

Then, the likely culprit is contention between access to ETH registers and GPIO registers on the AHB1 bus, see item 2 in my very first reply in this thread.

And there’s probably no workaround for that, except for the trivial one (not using ETH).

JW

PHolt.1
PHolt.1Author
Senior
Jul 3, 2026 12:54 PM UTC


#if (LCD_PAR8 && LCD_PAR8_DMA)

// TIM8 + DMA hardware /WR. CPU is idle during each burst.
//
// PC8 is a GPIO output (idle high) on entry. Flip it to AF3 (TIM8_CH3) for
// the pixel burst, then back to GPIO output afterwards so the next column's
// address setup can bit-bang /WR.
//
// Stream the buffer in <=256-byte bursts (RCR is 8-bit). Byte 0 of each burst
// is PRIMED BY THE DMA via a CC4G software event (TIM8 still stopped), not by
// a CPU write. That lets the DMA read from buffer[0] - which is 4-aligned -
// so MSIZE can be 32-bit (LCD_PAR8_DMA_M32): the FIFO reads one word and
// unpacks it 4:1 (little-endian, increasing address order) to the 8-bit
// peripheral side. The byte stream to the panel is IDENTICAL to the byte path
// because the buffer is already stored in send order; the 32-bit read only
// changes how memory is fetched, not what reaches PD8-15. PSIZE is always 8
// (the panel bus is 8-bit). One /WR per byte either way.
//
// SEQUENCE per burst:
// 1. Arm DMA: source = b[0], NDTR = n (the FULL byte count), stream enabled.
// 2. Enable CC4DE.
// 3. Fire TIM8->EGR = CC4G with the timer STILL STOPPED. This generates one
// CC4 event -> one DMA request -> DMA stores byte 0 to ODR+1. NDTR -> n-1.
// __DSB() so that store reaches the bus before the timer can latch it.
// 4. Clear CC4IF (the EGR-CC4G just set it); if left set, starting CC4DE/the
// timer would fire a spurious request and shift the burst by one byte.
// 5. Load RCR = n-1 (n /WR pulses total: pulse 0 latches the primed byte 0,
// pulses 1..n-1 latch the DMA-loaded bytes 1..n-1).
// 6. Start the timer (CEN). Each subsequent CC4 (at CCR4, while /WR is high)
// loads the next byte, settling before the next latch.
//
// COMPLETION: wait on TCIF7 (transfer complete), consistent with the SPI3/SPI1
// DMA code in SPI.c which deliberately prefers the transfer-complete flag
// over NDTR (NDTR can read back unreliably mid-transfer; see the efton g20
// gotcha). TCIF7 was freshly cleared by the HIFCR write when this burst was
// armed, so it reflects THIS transfer. Error flags also break the wait so an
// errored transfer cannot hang. Bounded by a guard.
//
// HANG SAFETY: every spin is bounded by a ~100k guard; a missed stop or DMA
// error degrades to a dropped/short line, never a task hang. The counters
// g_lcd_par8_dma_timeout1/2/3 record which guard tripped.
// The 1st 2 timeouts have never occurred but g_lcd_par8_dma_timeout3 does.

LCD_DC_GPIO_PORT->BSRR = LCD_DC_PIN; // DAT: D/C=1
lcd_cs(0);

// PC8 -> AF3 (TIM8_CH3): the timer drives /WR for the DMA burst.
GPIOC->MODER = (GPIOC->MODER & ~(3u << (8*2))) | (2u << (8*2)); // PC8 = AF

uint32_t off = 0;
while (off < size)
{
uint32_t n = size - off;
if (n > 256u) n = 256u;
const uint8_t *b = &outbuf[off];

// CC4 DMA request OFF while we set up.
TIM8->DIER &= ~TIM_DIER_CC4DE;

// Arm DMA for the WHOLE burst: bytes 0..n-1 from b[0].
uint32_t guard;
DMA2_Stream7->CR &= ~DMA_SxCR_EN;
guard = 100000u;
while ((DMA2_Stream7->CR & DMA_SxCR_EN) && --guard) { }
if (guard == 0u) g_lcd_par8_dma_timeout1++;
DMA2->HIFCR = (DMA_HIFCR_CTCIF7 | DMA_HIFCR_CHTIF7 |
DMA_HIFCR_CTEIF7 | DMA_HIFCR_CDMEIF7 | DMA_HIFCR_CFEIF7);
DMA2_Stream7->M0AR = (uint32_t)&b[0];
DMA2_Stream7->NDTR = n;
DMA2_Stream7->CR |= DMA_SxCR_EN;

// Load RCR (n pulses) via UG with CC4DE OFF, then clear UIF/CC4IF.
TIM8->RCR = n - 1u;
TIM8->EGR = TIM_EGR_UG;
TIM8->SR = 0;

// Enable CC4 DMA, then PRIME byte 0 by firing a CC4 event while the timer
// is still stopped: this makes the DMA store byte 0 to ODR+1 now.
TIM8->DIER |= TIM_DIER_CC4DE;
TIM8->EGR = TIM_EGR_CC4G; // software CC4 event -> one DMA request (byte 0)
__DSB(); // byte 0 store committed before the timer starts

// The CC4G just set CC4IF; clear it so starting the timer does not fire a
// spurious extra request (which would shift the burst by one byte).
TIM8->SR = 0;

// Start the timer. Pulse 0 latches the primed byte 0; CC4 at CCR4 each
// period loads the next byte while /WR is high.
TIM8->CR1 |= TIM_CR1_CEN;

// This function can contain whatever (state machine etc) can be done usefully
// during the 20us or so of the AI column draw
if (call_dead_time_function) dead_time_function();

// Wait for OPM to self-stop the timer (bounded).
guard = 100000u;
while ((TIM8->CR1 & TIM_CR1_CEN) && --guard) { }
if (guard == 0u) g_lcd_par8_dma_timeout2++;

// Wait for the DMA to finish transferring its last byte before disabling it.
// This sometimes does not happen because there is a rare timer->DMA latency
// due to some unknown bus arbitration issue. ETH is a factor but not the only
// one. When a CC4 trigger is missed this way, that /WR pulse latches a REPEAT
// of the previous byte (ODR wasn't updated in time), so the DMA ends up one
// load short: the byte count sticks at 1 and TCIF7 never sets - the trigger
// that would have cleared it is already in the past, so waiting longer cannot
// help. The timeout below is therefore the correct bounded give-up, not a
// failed wait: it abandons the stranded byte and disables the stream. The
// visible result is ONE duplicated pixel-byte on that line (not a short/torn
// line), self-healing on the next full redraw. The error count directly
// records these rare long-latency events; over a 10h ETH-running soak it was
// ~72, i.e. ~1 in 10M bursts, invisible on a continuously-redrawn display.

uint32_t guard3 = 100000u;
while (!(DMA2->HISR & (DMA_HISR_TCIF7 | DMA_HISR_TEIF7 |
DMA_HISR_DMEIF7 | DMA_HISR_FEIF7)) && --guard3) { }
if (guard3 == 0u) g_lcd_par8_dma_timeout3++;
DMA2_Stream7->CR &= ~DMA_SxCR_EN;

TIM8->DIER &= ~TIM_DIER_CC4DE;

off += n;
}

// Very rarely the above PWM gen leaves /wr=0 so setting it to 1 below creates
// a +ve edge. OPM stops TIM8 at CNT=0, in the LOW half of the PWM mode-2
// cycle, so CH3 leaves /WR (PC8, still AF) driven LOW. Flipping PC8 to GPIO-
// high here would drive /WR low->high while /CS is STILL LOW - a spurious
// rising edge latching one extra pixel. So deselect FIRST: raise /CS while
// /WR is still (harmlessly) low, THEN bring /WR back to idle-high.
lcd_cs(1); // /CS = 1 FIRST (deselect)

GPIOC->BSRR = WR_C_HIGH; // PC8 ODR = 1
__DSB(); // /WR-high store committed before PC8 leaves AF
GPIOC->MODER = (GPIOC->MODER & ~(3u << (8*2))) | (1u << (8*2)); // PC8 -> GPIO output (now follows ODR = high)
__DSB(); // ensure PC8 is GPIO before any following bit-bang

The only thing I recognise in that table as being applicable is DMA1 or DMA2.

This is the DMA code. Would the poll of the status reg interfere so badly with it? I did try padding it with a load of NOPs but it made no difference.

DMA1 is used for SPI3, none of which runs faster than 10.5MHz clock, so fairly rare accesses.