Skip to main content
sam239955
Associate III
May 27, 2013
Question

STM32F4 with external NAND-Flash - whats the Adress Area?

  • May 27, 2013
  • 1 reply
  • 769 views
Posted on May 28, 2013 at 01:00

Hi,

I'm using this Board: http://www.keil.com/support/man/docs/mcbstm32f200/mcbstm32f200_to_memory.htm

to build up a small webserver interface. I want to put the website data on the NAND-Flash. But what is the Adress of the Area? Why KEIL wrote ''Not directly mapped to a memory area''.

How can I access the memory then?

please help.

Alex

#flash #nand #adress
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
May 28, 2013
Posted on May 28, 2013 at 02:40

NAND is not ''mapped'' into memory in the regular sense, so you can't memcpy() or whatever directly to it in a random-access fashion. It acts more like a hard drive (block device), there are addresses to send COMMAND, ADDRESS and DATA values, and these select blocks/pages within the larger NAND array, and permit the retrieval of data situated there.

The DATA register is at 0x80000000, the ADDR 0x80020000, CMD 0x80010000, as best I can tell from the example files.

The way the address is configured to the device, it will not see low order address bits, a memcpy(holdbuf, 0x80000000, 0x10000); will effectively stream 64KB out of the NAND as it will look like a repetitive access to the DATA register.

Also note with an address space of less than 256KB you could access a device potential holding several GB of memory, which could well exceed the 4GB limit of a 32-bit address bus.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..