stm32f4 Virtual Comm not talking to custom app
I am working with the STM32f4 Virtual Comm (code generated by the stmCube). I was able to communicate with my custom app written in c# with visual studio 2012; however, recently it stops communicating with the App. it throws an exception 'This parameter is incorrect'. i don't believe my firmware is wrong because i can communicate just fine with Tera Term also, I don't believe my c# code is incorrect because I can open other comm port with it.
is there a bug in visual studio serial port?
this is my c# serial init code:
serial_port.PortName = port;//this is 'COM3'
serial_port.DataBits = 8; serial_port.Parity = Parity.None; serial_port.StopBits = StopBits.One; serial_port.BaudRate = 112500; serial_port.Handshake = Handshake.None;// Set the read/write timeouts
serial_port.ReadTimeout = 1000; serial_port.WriteTimeout = 1000; serial_port.ReadBufferSize = 1024; serial_port.WriteBufferSize = 1024;