STM32F4 USB Virtual Com Port weird problem/settings solved?
Hey there,
I am trying to put up a VCP for Nucleo144 STM32F429 and had hard time figuring out why i cannot connect with my Terminal Program board with the CubeMX generated Sourcecode.
I dont know why but this worked for me now:
In CubeMX:
Board Selection->STM32->Nucleo144->F429ZI
Pinout Tab:
Peripherals:
USB_OTG_FS->Device Only
RCC->Enable HSE->Bypass
MiddleWares:
Enable USB_DEVICE->Communication Device Class(Virtual Com Port)
Clock Configuration:
PLL Source Mux: HSE 8MHz /M= 4, *N = 168, /P = 2, /Q =7
System Clock Mux: PLLCLK-> 168MHz
APB1 peripheral clocks 42 MHz
Configuration Tab:
Connectivity->USB_FS->Parameter Settings->VBUS Sensing-> Disabled
Project Settings->Linker Settings:
Heap from 0x200 to 0x2000
Stack from 0x400 to 0x600
Project Settings
In IAR Embedded Workbench:
USB_HS_MAX_PACKET_SIZE from 512 to 256
CDC_DATA_HS_MAX_PACKET_SIZE from 512 to 256
(this doesnt really affected the problem so i changed it back to 512 since im using FS-mode)
Still I cannot connect via a Terminal from Host PC.
So i searched and now this happens:
Back in CubeMX taking a harder look at USB_DEVICE in Configuartion Tab.
I changed USBD_MAX_STR_DESC_SIZ the default 512 to 64 bytes, because description says between 1 and 64. Why default is 512 then?
->Still cannot connect.
Changed USBD_DEBUG_LEVEL to 3.
I finally can connect to device via Terminal.
I will try to rebuild this scenario tomorrow to see if this option really making me that trouble.
Could these settings have such impact on the right configuration?