Visitor II
April 19, 2017
Question
STM32f4 USB HS HAL Driver bugs
- April 19, 2017
- 5 replies
- 1927 views
Posted on April 19, 2017 at 23:28
Hello.
I'm working on application of USB communication with high speed (about 50 Mbit/s). So I used ULPI PHY.
For some purpose I used CubeMX (v 4.20.1) and was surprising that my application didn't work. Enabling DMA on USB controller crashed all communications but I needed it for high speed. I started to trace the code and found some bugs in HAL Driver:
1. DMA doesn't enable properly.
2. Dedicated interrupts for endpoint1 doesn't set properly.
After I fixed these bugs my application started work properly. I can't find any mention of resolving the same problem in the Internet and I hope that my information is helpful.
I attached two patches for stm32f4xx_hal_pcd.c and stm32f4xx_ll_usb.c files to this message.
#bug #hal-bug