Skip to main content
thommagn
Associate II
October 18, 2012
Question

STM32F4 Usart1 problem

  • October 18, 2012
  • 7 replies
  • 1409 views
Posted on October 18, 2012 at 11:01

Hi,

Im using a STM32f405RG and i am trying to get a simple USART example to work. I load the following code to the mcu:

#include ''stm32f4xx.h''
#include ''stm32f4xx_gpio.h''
#include ''stm32f4xx_usart.h''
#include ''stm32f4xx_rcc.h''
void init_usart(void){
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* enable peripheral clock for USART2 */
RCC_APB1PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
/* GPIOA Configuration: USART1 TX on PA9 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect USART1 pins to AF9 */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1);
USART_InitStructure.USART_BaudRate = 57600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE); // enable USART2
}
void Delay(__IO uint32_t nCount)
{
while(nCount--)
{
}
}
int main(void){
init_usart();
while(1){
USART_SendData(USART1, 'h'); 
Delay(0x3FFFFF);
}
}

when

GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1);

is executed, the pin goes high, and nothing else happens.. The pin never resets and there is no data transmitted over the usart. Have anyone seen anything like this before? EDIT: If I change the code to work with USART2 everything works.. I wonder if it may have something to do with the

RCC_APB2Periph_USART1.

Im not very familliar with this and how the USART behaves if it's incorrect set. I'm also using CooCox.

/Tom
    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    October 18, 2012
    Posted on October 18, 2012 at 13:13

    RCC_APB1PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

    Not APB1
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    David Littell
    Senior II
    October 18, 2012
    Posted on October 18, 2012 at 13:41

    I thought peripherals like that were either on one bus or the other, so how did his error even compile?

    Tesla DeLorean
    Guru
    October 18, 2012
    Posted on October 18, 2012 at 14:02

    I thought peripherals like that were either on one bus or the other, so how did his error even compile?

    Because the syntax is correct, the preprocessor substitutes a bit vector, it's not an enum, and it cares not about which bus it relates too.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    thommagn
    thommagnAuthor
    Associate II
    October 18, 2012
    Posted on October 18, 2012 at 15:46

    Hi, thanks for the input. I can't belive I made such a stupid mistake, have been working with USART2-4 only. Guess i got blind when trying to switch to USART1!

    I changed

    RCC_APB1PeriphClockCmd( ... 

    to

    RCC_APB2PeriphClockCmd( ...

    But the result is the same, the signal goes high and nothing else happens. 

    Have I made another mindblowing mistake I'm unable to see?

    / Tom

    Tesla DeLorean
    Guru
    October 18, 2012
    Posted on October 18, 2012 at 17:58

    You're using CooCox, does that count?

    Make sure you're looking at the right pin, and what it's connected too. PA9 has a big capacitor hung off it on the STM32F4-Discovery board, try 1200 baud?

    // STM32F405 USART1 (Tx PA.9, Rx PA.10) - sourcer32@gmail.com
    #include ''stm32f4xx.h''
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    /* --------------------------- System Clocks Configuration -----------------*/
    /* USART1 clock enable */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
    /* GPIOA clock enable */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /*-------------------------- GPIO Configuration ----------------------------*/
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* Connect USART pins to AF */
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1); // USART1_TX
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1); // USART1_RX
    }
    /**************************************************************************************/
    void USART1_Configuration(void)
    {
    USART_InitTypeDef USART_InitStructure;
    /* USARTx configuration ------------------------------------------------------*/
    /* USARTx configured as follow:
    - BaudRate = 9600 baud
    - Word Length = 8 Bits
    - One Stop Bit
    - No parity
    - Hardware flow control disabled (RTS and CTS signals)
    - Receive and transmit enabled
    */
    USART_InitStructure.USART_BaudRate = 9600;
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    USART_InitStructure.USART_Parity = USART_Parity_No;
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    USART_Init(USART1, &USART_InitStructure);
    USART_Cmd(USART1, ENABLE);
    }
    /**************************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    USART1_Configuration();
    while(1)
    {
    while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
    USART_SendData(USART1, 0x49); // Send 'I'
    }
    while(1); // Don't want to exit
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    thommagn
    thommagnAuthor
    Associate II
    October 18, 2012
    Posted on October 18, 2012 at 18:46

    About Coocox, probably not. I have an external oscilator on my chip, and i'm not sure that i've done everything correct adjusting for it. In fact, I have only defined HSE_VALUE to the frequency of my oscillator and executed the following commands at startup:

    RCC_HSEConfig(RCC_HSE_ON);

    RCC_WaitForHSEStartUp();

    So I didn't trust myself. 

    About the USART problem, your first suggestion was correct! I had my project outside coocox workspace, and for some reason I loaded the wrong elf-file onto the chip. The Idea of copying a project from coocox workspace to another location, then trying to debug that project is no go. (Probably it was I who did something wrong in this process,,.)

    /Tom

    Tesla DeLorean
    Guru
    October 18, 2012
    Posted on October 18, 2012 at 20:00

    The clock stuff usually resides in SystemInit() in system_stm324xx.c

    To run from HSE you must select it as a source once you have it running.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..