Skip to main content
elec_st
Associate III
October 21, 2016
Question

stm32f4 to stm32f103

  • October 21, 2016
  • 1 reply
  • 803 views
Posted on October 21, 2016 at 10:06

i have stm32f407 discovery board and the  stm32f407 is damage

but i have stm32f103vct6 100pin chip

can i replace  stm32f407  by  stm32f103vct6 ?????

i know there is pin different can i solve it ?

 
    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    October 21, 2016
    Posted on October 21, 2016 at 10:44

    Hello,

    I recommend you to take a look to the Application note

    http://www.st.com/content/ccc/resource/technical/document/application_note/group0/e9/c4/6b/99/4e/d3/4e/a0/DM00325582/files/DM00325582.pdf/jcr:content/translations/en.DM00325582.pdf

    ''Migration of microcontroller applications from STM32F1 Series to STM32F4 Access lines''. 

    This reference can help you to determine differences between the two series with give attention to pinout, peripherals and system clock...

    You can refer to the document under

    http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32f1-series/stm32f103/stm32f103vc.html

     page, start from the template project in the

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubef1.html

    package and then add your own update.

    The migration for the HAL library is easily from one device to another as functions' names are the same for all series.

    Regards