Skip to main content
jagdish
Associate II
August 27, 2014
Question

STM32f4 SPI spurious Interrupt problem

  • August 27, 2014
  • 1 reply
  • 681 views
Posted on August 27, 2014 at 09:47

Hello,

Kindly help me resolve the STM32F4 SPI interrupt problem.

I am trying to connect two stm32f4 boards, one of it is stm32f439 evaluation board and other one is stm32f407 based my development board. I am testing interrupt based SPI communication example. I am using SPI1 peripheral for both boards. I have configured STM32F439 eval board as Master and my STM32F407 based dev't board as slave. 

Have enabled Rx interrupt on slave board. I have grounded SPI slave cs pin and have configured slave with SPI_NSS_Soft setting.

I am expecting that when i start transferring data from master board, slave board should invoke SPI rx interrupt ISR.

But here what i observed is that as soon as my slave board boots up it gets SPI receive interrupt. It doesn't wait for master to send data. I tried this even without connecting Master card signals to Slave card.

I am unable to understand what triggers the SPI interrupt. Is it a setting problem or hardware problem

I understand that when rx data register is not empty, Rx interrupt will occur

Kindly help.

#stm32 #stm32f4-spi-interrupt
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
August 27, 2014
Posted on August 27, 2014 at 13:04

Review : STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Project\STM32F4xx_StdPeriph_Examples\SPI\SPI_TwoBoards\SPI_DataExchangeInterrupt\readme.txt

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..