Skip to main content
Stephan Scherer
Associate III
May 2, 2018
Question

STM32F4 RTC problem

  • May 2, 2018
  • 0 replies
  • 463 views
Posted on May 02, 2018 at 14:51

Hello,

I have a problem. I use a STM32F427 with Keil RTX.

If I start my Programm without a backup battery my Programm runs into a rtos error (stack Overflow) if I want to set the date/time, but at this time the os isn't running.

I use an external 32768 Hz oscillator as LSE clock.

Can anyone give me a hint what I can do to solve this problem?

If I have a battery connected the Programm works fine at the second start, if there is a date/time in the system.

Best regards

Stephan

    This topic has been closed for replies.