Skip to main content
prog
Associate
Jul 29, 2016 11:19 AM UTC
Question

STM32F4 LTDC - scan lines

Posted on July 29, 2016 at 13:19

Hi All,

My hardware is custom STM32F429 board with 7'' TFT.

Display has no U/D or R/L display mode select pin.

I don't see datasheet LTDC registers to configure scanning order.

Actually i do it manually in software, perhaps using DMA2D will be quicker but still is to slowly

There is some idea to setup it ?

Andrew

    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    Jul 29, 2016 12:52 PM UTC
    Posted on July 29, 2016 at 14:52

    Hi,

    You can have a look to the LTDC examples under STM32CubeF4 package, it maybe helpful for you:

    STM32Cube_FW_F4_V1.13.0\Projects\STM324x9I_EVAL\Examples\LTDC\LTDC_Display_2Layers

    This example can be a starting point to learn about programming the display as it describes how to configure the LTDC peripheral to display two Layers at the same time. 

    You can also, refer to the 

    http://www.st.com/content/ccc/resource/technical/document/reference_manual/3d/6d/5a/66/b4/99/40/d4/DM00031020.pdf/files/DM00031020.pdf/jcr:content/translations/en.DM00031020.pdf

    , section 16 LCD-TFT controller (LTDC)

    Regards