Skip to main content
Yiran Tian
Visitor II
March 24, 2017
Question

STM32F4 having trouble into SLEEP mode

Posted on March 24, 2017 at 11:03

Hello there,

Currently I'm using a STM32F407VG discovery board to testing the stm32 low power features. STM32CubeMX was used to generate a simple demo. However, it seems always not able to enter sleep mode (standby mode tested, same story). 

Its a simple program, all peripherals and clock are remain in reset state. The main function looks like this:

 int main(void)

{

    HAL_Init();

    SystemClock_Config();

    HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);

   while(1)

   {

   }

}

Its for sure code will goes to while(1) segment and not enter SLEEP mode. I've done some readings and say Systick can cause the problem. So I add code below right before calling HAL_PWR_EnterSLEEPMode();

// disable SysTick

SysTick->CTRL = 0x00000004;

And most of time MCU can get into low power mode, but still, miss one or two shot out of few tests. 

So my questions are as below:

1. Do I have to close SysTick before WFI? If not, which part have I missed?

2. Datasheet saying that any pending/activated interrupt will cause not able to into SLEEP mode. However I'm running this code in main(), not IRQ handler. In that case nothing could block me from entering SLEEP mode correct?

3. Same story entering STANDBY mode as SLEEP. What have I missed?

4. I've tried put HAL_PWR_EnterSLEEP() into while(1) block. Without disable SysTick, it never trigger SLEEPMODE.

Appreciate for your reply in advance!! Really looking forward to get response soon

Regards,

Tien 

#low-power #sleep-mode
This topic has been closed for replies.

2 replies

Nesrine M_O
Associate
March 24, 2017
Posted on March 24, 2017 at 11:46

Hi

rye02

,

I recommend you to start from ready example under the STM32F4 firmware package :

STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Examples\PWR

-Nesrine-

Associate III
April 15, 2025

@Yiran Tian I am also facing a similar issue like this. For TouchGFX application, I am trying to implement sleep mode, HAL_SuspendTick() is working fine (cross verified by using HAL_Delay()after the suspendTick() , not working as time base which is responsible for producing HAL_Delay() is disabled) after the HAL_SuspendTick() function call, the control is expected to stop at _WFI, present inside the HAL_PWREnableSLEEPMode()'s function definition, but it is not stopping and waiting for interrupt. Kindly help me to solve my issue.

Thank You,

Abhiram_12_1-1744694065266.png