Question
STM32F4 Hal drivers. Problem reading a songle byte with HAL_I2C_Mem_Read_IT
Posted on August 17, 2016 at 11:35
Hello,
when I read a single Byte from I2C using the HAL_I2C_Mem_Read_IT function, all following read or write attempts on the same I2C bus fail with HAL_Timeout.
When I run exactly the same code on a STM32F2 (using the F2 HAL Drivers) I have no Problems.
Do you have any idea what could cause this issue?