Skip to main content
alem_sd
Associate
October 28, 2013
Question

STM32F4 Generation PWM

  • October 28, 2013
  • 3 replies
  • 845 views
Posted on October 28, 2013 at 11:06

Please!

Help me to generate a meander with frequency of 8 MHz on the timer - counter in mode PWM. Clocking from MCO1/MCO2 does not approach!
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    October 28, 2013
    Posted on October 28, 2013 at 12:36

    Blind modification of previously posted example

    // STM32 PWM 8 MHz (TIM1 CH1 PA.08) STM32F4 Discovery - sourcer32@gmail.com
    #include ''stm32f4_discovery.h''
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    /* --------------------------- System Clocks Configuration -----------------*/
    /* TIM1 clock enable */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
    /* GPIOA clock enable */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /*-------------------------- GPIO Configuration ----------------------------*/
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* Connect TIM1 pins to AF */
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1);
    }
    /**************************************************************************************/
    void TIM1_Configuration(void)
    {
    TIM_OCInitTypeDef TIM_OCInitStructure;
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    uint16_t Period;
    Period = (SystemCoreClock / 8000000);
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Prescaler = 0; // Dump 1X clock into timer
    TIM_TimeBaseStructure.TIM_Period = Period - 1;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
    /* TIM PWM1 Mode configuration */
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    /* Output Compare PWM1 Mode configuration: Channel1 PA.08 */
    TIM_OC1Init(TIM1, &TIM_OCInitStructure);
    /* TIM1 Main Output Enable */
    TIM_CtrlPWMOutputs(TIM1, ENABLE);
    /* TIM1 enable counter */
    TIM_Cmd(TIM1, ENABLE);
    }
    /**************************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    TIM1_Configuration();
    while(1); // Don't want to exit
    }
    /**************************************************************************************/
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {
    }
    }
    #endif
    /**
    * @}
    */
    /**************************************************************************************/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    alem_sd
    alem_sdAuthor
    Associate
    October 29, 2013
    Posted on October 29, 2013 at 08:08

    Many thanks for the help! I have started on Discovery - and all right.

    But it is necessary for me to use pin PA7. On it the inverse signal from  TIM1-CH1N comes - and there 8 MHz is not present!

    Tesla DeLorean
    Guru
    October 29, 2013
    Posted on October 29, 2013 at 16:24

    // STM32 PWM 8 MHz (TIM1 CH1 PA.08, CH1N PA.07) STM32F4 Discovery - sourcer32@gmail.com
    #include ''stm32f4_discovery.h''
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    /* --------------------------- System Clocks Configuration -----------------*/
    /* TIM1 clock enable */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
    /* GPIOA clock enable */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /*-------------------------- GPIO Configuration ----------------------------*/
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* Connect TIM1 pins to AF */
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1); // PA.08 TIM1_CH1
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_TIM1); // PA.07 TIM1_CH1N
    }
    /**************************************************************************************/
    void TIM1_Configuration(void)
    {
    TIM_OCInitTypeDef TIM_OCInitStructure;
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    uint16_t Period;
    Period = (SystemCoreClock / 8000000);
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Prescaler = 0; // Dump 1X clock into timer
    TIM_TimeBaseStructure.TIM_Period = Period - 1;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
    /* TIM PWM1 Mode configuration */
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
    TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;
    TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable;
    TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High;
    TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;
    /* Output Compare PWM1 Mode configuration: Channel1 PA.08/PA.07 */
    TIM_OC1Init(TIM1, &TIM_OCInitStructure);
    /* TIM1 Main Output Enable */
    TIM_CtrlPWMOutputs(TIM1, ENABLE);
    /* TIM1 enable counter */
    TIM_Cmd(TIM1, ENABLE);
    }
    /**************************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    TIM1_Configuration();
    while(1); // Don't want to exit
    }
    /**************************************************************************************/
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {
    }
    }
    #endif
    /**
    * @}
    */
    /**************************************************************************************/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..