Skip to main content
Kuikui
Associate III
June 30, 2016
Question

STM32F4 FMC on non-multiplexed SRAM

  • June 30, 2016
  • 1 reply
  • 521 views
Posted on June 30, 2016 at 11:55

Hi,

I plan to build a board with an STM32F446VE + IS66WV51216EBLL

As the STM32F446VE is a 100pin package, it does not offer non-multiplexed interface on the FMC.

So I was considering using the FMC in multiplexed PSRAM mode, and adding a latch like the 74LVC373AD device (to transform the multiplexed interface to non-multiplexed interface), but it seems that the FMC_NL ( = NADV ) line is inverted ..

Couldn't find if it was possible to invert FMC_NL logic, so I suppose I can't.

Consequently, it seems I should add an inverter before the latch.

Sounds tricky in the end, and as I couldn't find any example on the internet of someone using the multiplexed FMC on non-multiplexed PSRAM, I wonder is this can really work ..

Any advice ?

Thanks and best regards,

Vincent.

#stm32f4 #sram #- #fmc
This topic has been closed for replies.

1 reply

Kuikui
KuikuiAuthor
Associate III
July 5, 2016
Posted on July 05, 2016 at 13:48