STM32F4 DMA FIFO + SPI_TX = FIFO error, but work
Good afternoon! I am trying to establish the transmission of data via SPI to the display with DMA. The transmission is working, the display is completely painted over, but the FIFO error flag is set in the DMA registers.
MCU: STM32F401CEU6
alignas(32) uint16_t buff[80 * 160];
// SPI init
SPI2->CR1 |= (0b000 << SPI_CR1_BR_Pos) |
SPI_CR1_MSTR |
SPI_CR1_SSI | SPI_CR1_SSM;
SPI2->CR2 |= SPI_CR2_TXDMAEN;
SPI2->CR1 |= SPI_CR1_SPE;
// DMA init
DMA1_Stream4->CR |= (0b01 << DMA_SxCR_DIR_Pos) |
(0 << DMA_SxCR_CHSEL_Pos) |
(0b11 << DMA_SxCR_MBURST_Pos) |
DMA_SxCR_MINC;
DMA1_Stream4->PAR = (uint32_t)&SPI2->DR;
DMA1_Stream4->M0AR = (uint32_t)getBuffer();
DMA1_Stream4->FCR &= ~DMA_SxFCR_FTH;
DMA1_Stream4->FCR |= DMA_SxFCR_DMDIS;
__DMB();
DMA1_Stream4->FCR |= (0b11 << DMA_SxFCR_FTH_Pos);void ST7735s::stopScreenUpdate()
{
DMA1_Stream4->CR &= ~DMA_SxCR_EN;
while (DMA2_Stream4->CR & DMA_SxCR_EN)
;
CS_Up();
}
void ST7735s::startScreenUpdate()
{
stopScreenUpdate();
sendCommand(ST77XX_RAMWR);
CS_Down();
DC_Up();
DMA1->HIFCR = DMA_HIFCR_CFEIF4 | DMA_HIFCR_CHTIF4 | DMA_HIFCR_CTCIF4 | DMA_HIFCR_CTEIF4 | DMA_HIFCR_CDMEIF4;
DMA1_Stream4->NDTR = WIDTH * HEIGHT * 2;
DMA1_Stream4->CR |= DMA_SxCR_EN;
}After transmission, the FIFO buffer operation error flag in DMA is set. The flag has to be reset manually + it's not normal somehow.
- 80 pixels * 160 pixels * 2 bytes = 25,600 bytes. In total, if I understood the logic correctly, with a packet size of 16 chunks, with a chunk size = MSIZE = 1 byte, everything should work, because the configuration is allowed + 25,600 bytes exactly divided into transactions of 16 bytes.
- I tried to change NDTR - divided by 16, but it didn't help, because it is necessary to specify exactly the number of bytes transmitted. With division by 16, only 1/16 of the display is filled.
- There is no overwriting (ovverun) either - all pixels take their places
- There are no SPI errors (Except overrun, since I only use sending)
The alignment was done with a margin. Tried before 4 - no result