Question
STM32F4 Discovery UART DMA TX Problem
Posted on June 06, 2014 at 00:52
Hey ST Forum,
I'm using the ST32F4-Discovery Board, and ran into some problems while testing UART4_TX in DMA Mode. When I look at oscilloscope, the TX line is pulled down, then gradually goes back to 3V. I think my Peripheral and base addresses are set wrong (bold below). Please give me any ideas://6.5.14 UART DMA TRY//PC10 UART4_TX//Non-functional 6.5.14 - check line 66, 68#include ''stm32f4xx_gpio.h''#include ''stm32f4xx_rcc.h''#include ''stm32f4xx_usart.h''#include ''stm32f4xx_dma.h''//prototypesvoid RCC_Config(void);void GPIO_Config(void);void UART4_Config(void);void DMA_Config(void);//global variables#define UART4_TX_AD 0x000000;uint16_t hi[] = {1,2,3}; //checkint main(void){ RCC_Config(); GPIO_Config(); UART4_Config(); DMA_Config(); while(1) { }}void RCC_Config(void){ RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1 | RCC_AHB1Periph_GPIOC, ENABLE);}void GPIO_Config(void){ GPIO_InitTypeDef gpio; gpio.GPIO_Pin = GPIO_Pin_10; gpio.GPIO_Mode = GPIO_Mode_AF; gpio.GPIO_PuPd = GPIO_PuPd_NOPULL; gpio.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC,&gpio); GPIO_PinAFConfig(GPIOC,GPIO_PinSource10,GPIO_AF_UART4); //TX}void UART4_Config(void){//19.2kbaud, 8 bits, one stop, no parity USART_InitTypeDef usart; usart.USART_BaudRate = 19200; usart.USART_WordLength = USART_WordLength_8b; usart.USART_StopBits = USART_StopBits_1; usart.USART_Parity = USART_Parity_No; usart.USART_HardwareFlowControl = USART_HardwareFlowControl_None; usart.USART_Mode = USART_Mode_Tx; USART_Init(UART4,&usart);}void DMA_Config(void){//dma stream 4 channel 4, uart4_tx DMA_InitTypeDef dma; dma.DMA_Channel = DMA_Channel_4; dma.DMA_DIR = DMA_DIR_MemoryToPeripheral; dma.DMA_Memory0BaseAddr = (uint32_t)&hi;dma.DMA_BufferSize = 1; //? dma.DMA_PeripheralBaseAddr = (uint32_t)&UART4->DR; //Is this uart4 receive or transmit data register?
dma.DMA_PeripheralInc = DMA_PeripheralInc_Disable; dma.DMA_MemoryInc = DMA_MemoryInc_Enable; dma.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; //don't know dma.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; dma.DMA_Mode = DMA_Mode_Circular; //??? Circular vs Normal mode? dma.DMA_Priority = DMA_Priority_Medium; dma.DMA_FIFOMode = DMA_FIFOMode_Disable; dma.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; dma.DMA_MemoryBurst = DMA_MemoryBurst_Single; dma.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA1_Stream4,&dma); DMA_Cmd(DMA1_Stream4,ENABLE); USART_DMACmd(UART4,USART_DMAReq_Tx,ENABLE);}