Question
STM32F4 Discovery stuck waiting for PLL in uVision simulation
Posted on November 07, 2013 at 01:30
Hi
I am migrating a project to the STM32F4 Discovery and have managed to strip the Template program down to it�s minimum components as a base but have come up against a strange problem.I can run the original Template program (and the cut down version) OK but when I try to run them under Keil�s uVision Simulator mode they get stuck waiting for the PLL to come ready. Is there any way to fix this or should I just rem that out whilst using the debugger?Another anomaly running simulator is the need to allocate the memory 0x40000000, 047FFFFFF (which I think is part of the IO memory space) to read write but I got around that by allocating it in the debug.ini file.uVision V4.72.10.0 #stm32f4-discovery-pll-error-65