Skip to main content
dpfeffer9
Associate II
April 4, 2013
Question

STM32F4 Discovery: ST-LINK bricked

Posted on April 04, 2013 at 14:38

Hello,

out of a working setup, suddenly I dont get any connection to my ST-LINK anymore And LD1 is blinking red (f ~ 0.5 Hz). PA13/14 are not used in my program.

Even in Device-Manager there is no ST-LINK recognized anymore. Another Discovery board works perfectly.

What can I do to reanimate my precious STM32F4?

    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    April 4, 2013
    Posted on April 04, 2013 at 16:20

    If your code is causing a problem pulling BOOT0 High at start up will remove it from being an issue.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    dpfeffer9
    dpfeffer9Author
    Associate II
    April 4, 2013
    Posted on April 04, 2013 at 16:49

    thanks for the reply. i tried that, but it didn't work. Maybe the ST-Link Controller is defective?

    Tesla DeLorean
    Guru
    April 4, 2013
    Posted on April 04, 2013 at 16:54

    Perhaps, or may be you changed something. Like drivers, or installed something else? Moved some jumpers? Add circuitry, damaged a regulator?

    You could try on another system with a fresh install, or try a different discovery on the same system.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    dpfeffer9
    dpfeffer9Author
    Associate II
    April 5, 2013
    Posted on April 05, 2013 at 08:21

    Unfortunately, another identical F4-Discovery works with same setup, jumper-config and USB-cable...

    I cannot rule out a surge peak on any pin due to ESD, or that I accidentially touched a pinhead with 5 VDC.

    Is there any possibility to reflash the ST-LINK part of a discovery board?

    omermiranda
    Visitor II
    May 3, 2013
    Posted on May 03, 2013 at 05:44

    Hi,

    Windows 7 does not detect my STM32F0 discovery board. I am getting the following error:

    Windows has stopped this device because it has reported problems. (Code 43)

    It was working fine and all of a sudden its not getting detected.

    Any resolution??

    omermiranda
    Visitor II
    May 3, 2013
    Posted on May 03, 2013 at 05:45

    Hi,

    Windows 7 does not detect my STM32F0 discovery board. I am getting the following error:

    Windows has stopped this device because it has reported problems. (Code 43)

    It was working fine and all of a sudden its not getting detected.

    Any resolution??