Skip to main content
bkdi
Associate II
Mar 11, 2014 1:34 AM UTC
Question

STM32F4-DISCOVERY LD8 lights whole time

Posted on March 11, 2014 at 02:34

LD8 LED is ON (USB over-current) regardless to program. Furthermore receiving data by UART3 using pin PC11 is impossible, but with PD9 works fine. Earlier 

I had no

problems

, and now

after connected the

board

to the computer

is something wrong. Please tell me what  can cause problems.

Thank you

    This topic has been closed for replies.

    2 replies

    Amel NASRI
    ST Technical Moderator
    Mar 11, 2014 8:24 AM UTC
    Posted on March 11, 2014 at 09:24

    - Did you bring any hardware update to the board?

    - Earlier

    I had no

    problems

         Do you mean before connecting USB?

         Could you share minimum helpful code to understand issue? (May be you forgot to enable clock)

    -Mayla

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    bkdi
    bkdiAuthor
    Associate II
    Mar 11, 2014 6:56 PM UTC
    Posted on March 11, 2014 at 19:56

    I have worked on the program, that received data from UART3 and sended it by USB OTG to PC. It worked fine for a few weeks. Before the last connection to PC by CN1, when I saw, that pin PC11 was damaged (reception don't work) and LD8 is on, I had updated the ST-Link firmware to 2.19. After update I worked with my board for some hours. When I connected the Discovery to PC next day, there was  problem described above.

    I think this is hardware problem (not in my code), because LD8 lights even if I clean flash memory using STM32 ST-Link Utility, but maybe there is some solution?