Skip to main content
baev_al
Associate III
August 31, 2014
Question

STM32F4-discovery LCD linking question

Posted on August 31, 2014 at 08:15

Dear friends.

Please help with the following error:

Error[Li005]: no definition for ''LTDC_LayerInit''

Here is the part of the program:

/* Initialize the LCD */

LCD_Init();

/* LCD Configuration */

LCD_LayerInit();

Both functions are located in the same stm32f429i_discovery_lcd.c file. Why LCD_Init() is ok and LCD_LayerInit() is not?

I use EWARM 7.2.

Thanks

    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    August 31, 2014
    Posted on August 31, 2014 at 11:12

    LTDC not LCD

    The missing function is actually in one of the library files, which needs to be part of your project.

    STM32F429I-Discovery_FW_V1.0.1\Libraries\STM32F4xx_StdPeriph_Driver\src\stm32f4xx_ltdc.c

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    baev_al
    baev_alAuthor
    Associate III
    August 31, 2014
    Posted on August 31, 2014 at 14:41

    Thanks, Clive1.

    Several others errors appeared and I added all required header and source files. But I still did not see anything on the screen. Bellow is the code. How can I learn to use LCD libraries? How can I find my mistake inside below code using debugger?

    /* Includes ------------------------------------------------------------------*/

    #include ''main.h''

    #include ''stm32f429i_discovery_lcd.h''

    #include ''stm32f4xx.h''

    #include ''stm32f4xx_ltdc.h''

    #include ''stm32f4xx_fsmc.h''

    /** @addtogroup Template

      * @{

      */

    int main(void)

    {

    /* Initialize the LCD */

    LCD_Init();  

    /* LCD Configuration */

    LCD_LayerInit();

    /* Enable LCD display */

    LCD_DisplayOn();

    /* Set foreground layer */

    LCD_SetLayer(LCD_FOREGROUND_LAYER);

    /* Clear the LCD */

    LCD_Clear(LCD_COLOR_WHITE);

    /* Set the LCD Back Color */

    LCD_SetBackColor(LCD_COLOR_WHITE);

    /* Set the LCD Text Color */

    LCD_SetTextColor(LCD_COLOR_BLUE);

    LCD_DisplayStringLine(LCD_LINE_0, (uint8_t *)'' STM324x9I-EVAL '');

    LCD_DisplayStringLine(LCD_LINE_1, (uint8_t *)'' Example on how to '');

    LCD_DisplayStringLine(LCD_LINE_2, (uint8_t *)'' use the IO Expander '');

        

      /* Infinite loop */

      while (1)

      {

      }

    }

    #ifdef  USE_FULL_ASSERT

    /**

      * @brief  Reports the name of the source file and the source line number

      *         where the assert_param error has occurred.

      * @param  file: pointer to the source file name

      * @param  line: assert_param error line source number

      * @retval None

      */

    void assert_failed(uint8_t* file, uint32_t line)

    {

      /* User can add his own implementation to report the file name and line number,

         ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

      /* Infinite loop */

      while (1)

      {

      }

    }

    #endif
    Tesla DeLorean
    Guru
    August 31, 2014
    Posted on August 31, 2014 at 19:51

    I'd probably start by testing/review the examples for the specific board I'm using rather than a different board.

    STM32F429I-Discovery_FW_V1.0.1\Projects\Peripheral_Examples\LTDC_Display_2Layers\readme.txt

    Then I'd evaluate what is being done differently between the two. Like configuration of pins, and external memory banks.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    baev_al
    baev_alAuthor
    Associate III
    September 1, 2014
    Posted on September 01, 2014 at 16:26

    Studding the example LTDC_Display_2Layers. How can I obtain the hex array of the picture (such as st_logo1.h)?

    Tesla DeLorean
    Guru
    September 1, 2014
    Posted on September 01, 2014 at 17:05

    Generating data as an include file is a pretty simple, I've coded quick applications to do such. There are other apps that do more specific BMP conversion, colour level stuff.

    http://www.segger.com/emwin-bitmap-converter.html

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    baev_al
    baev_alAuthor
    Associate III
    September 2, 2014
    Posted on September 02, 2014 at 07:24

    Thanks, Clive1.

    The program solved the question. However I changed

    const uint32_t ST_LOGO_1[19200] =

    { 0xFFFFFFFF, ...

    to

    const uint16_t ST_LOGO_1[38400] =

    { 0x3161,...