Question
STM32F4-discovery FreeRTOS
Posted on November 07, 2014 at 21:49
Dear friends.
I try to use freeRTOS on STM32F429I-DISCO. I want to create two tasks (blinking different leds) just to understand how the OS works. I use EWARM 7. When I compile the projects I have the following errors:
identifier�?__set_BASEPRI�? is underfined
function�?__ser_BASEPRI�? has no prototype
I used the files from STM32F429I-Discovery_FW_V1.0.1 package. I didn't find source file with such function.
What did I do wrong?
Thanks!