Question
STM32F4 - Discovery - Example ''Audio_playback_and_record''
Posted on November 08, 2013 at 10:28
Good morning,
i have a problem with the board STM32F4 - Discovery. I'm using the example ''Audio_playback_and_record'' for this board. I configured this example to read file from a media usb key ( i have uncommented the code #define MEDIA_USB_KEY) .To play a file .wav this example use the double buffering technical :1- play data with the function Audio_MAL_Play((uint32_t)buffer1, _MAX_SS) using DMA;2-store data in buffer2;3- play data with the function Audio_MAL_Play((uint32_t)buffer2, _MAX_SS) using DMA;4-store data in buffer1;My problem is that i want reduce the sizes of buffer1 and buffer2 because for me application with 512 byte ( size buffers, i have configured it in main.h file) i have a big latency. If I modify the sizes of buffer1 and buffer2 and the play function in this way: buffer1[_MAX_SS/2];buffer2[_MAX_SS/2];Audio_MAL_Play((uint32_t)buffer2, _MAX_SS/2);the code don't work and the file .wav is not played.How can i do to reduce the number of bytes played with the function Audio_MAL_Play((uint32_t)buffer2, _MAX_SS)?Thank a lot for your help.Fabrizio