Skip to main content
waheed901
Associate III
Nov 25, 2015 5:23 AM UTC
Question

STM32F4 Discovery board to PC interface

Posted on November 25, 2015 at 06:23

Hi everyone,

I just want to seek your guidance and help in accessing 12 signed 32 bit integers, which are calculated by using STM32F4 Discovery board, in my PC, through USB.

I read many codes/post on different forum and could not figure out from where to start. I am very much beginner with this board so need your help. 

These variables are constantly changing and I wish to access in real time. Can anyone help me in locating suitable example so that I can start.
    This topic has been closed for replies.

    4 replies

    Nickname5522_O
    Visitor II
    Nov 25, 2015 3:20 PM UTC
    Posted on November 25, 2015 at 16:20

    Hi w.a,

    I advise you to refer to 

    http://www.st.com/web/en/catalog/tools/PF257920

     and its 

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00196932.pdf

    .  It explains how to exchange data using the HID class protocols.

    Also, you can have a look to the example under STM32Cube_FW_F4_V1.9.0\Projects\STM324x9I_EVAL\Applications\USB_Device\CustomHID_Standalone.

    -Shahrzad-

    aaron239955_stm1_st
    Senior
    Nov 25, 2015 10:24 PM UTC
    Posted on November 25, 2015 at 23:24

    I would think the most natural way to do this would be to set up the USB peripheral as a virtual Comm port so the PC can receive data through what it thinks is a standard com: port.  I have several examples of using CubeMX with Coocox's free CoIDE development environment.  The second example shows how to get this working.  You can find them at:

    https://www.dropbox.com/sh/yg4iy7h6xmca7lk/AACouu73L44JaYNdtgqSV0pna?dl=0

    good luck.

    waheed901
    waheed901Author
    Associate III
    Nov 26, 2015 2:40 AM UTC
    Posted on November 26, 2015 at 03:40

    thank you very much for the replies. 

    Actually I am not comfortable with cubeMX and using firmware for my other projects, so interested if any one can help in some examples related to the interface in firmware

    thanks in advance

    waheed901
    waheed901Author
    Associate III
    Feb 1, 2016 3:32 AM UTC
    Posted on February 01, 2016 at 04:32

    I need your kind help in searching out some solution for sending data as output on STM32 pins and accessing it from the computer. 

    a).  I have 9 variables (16 bits), calculated in MCU and want to send them to output pins of STM32 board  (can you please share any example similar to this??)

    b).  Access them on computer by any mean (USB or serial port) 

    Please note that I just want to put some values on some pins of STM32 discovery board which can be read by the computer at any time. These values may be updated frequently but some check should be there that when computer is reading those values they should not be updated.

    Your help in this regard will be highly appreciated.