Skip to main content
shorai
Associate III
February 8, 2023
Solved

STM32F4 Disco RTC (old version) not updating SECONDS

I am using the Audio Playback and record exaample.

I modified Systeem_clock_config as follos

 /* Enable HSE Oscillator and activate PLL with HSE as source */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI | RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSIState = RCC_LSI_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

Then ran the RTC config from a Cube generated source

My main is stubbed out to do the following

 SystemClock_Config();
 
 
 /* Initialize MEMS Accelerometer mounted on STM32F4-Discovery board */
 if(BSP_ACCELERO_Init() != ACCELERO_OK)
 {
 /* Initialization Error */
 Error_Handler();
 }
 
 MemsID = BSP_ACCELERO_ReadID();
// RTC does not initiaalise with the system clock config dictated by this SW.
 // By not using the IOC file, it is a pain to debug the clock config errors
 // The ARM compiler optimisation also messes with the program flow
MX_RTC_Init();
 MX_DMA_Init();
 MX_USART2_UART_Init();
 
 HAL_RTC_MspInit(&hrtc);
 while (-1) {
	 RTC_TimeTypeDef ttime;
	 HAL_RTC_GetTime(&hrtc, &ttime, RTC_HOURFORMAT_24);
 char str[50];
 sprintf(str,"%5d %5d %5ld %5ld\r\n",ttime.Minutes,ttime.Seconds, ttime.SubSeconds,ttime.SecondFraction);
 HAL_UART_Transmit_DMA(&huart2,(uint8_t *) str,strlen(str));
 HAL_Delay(990);
 }

And my output on the serial port looks like this

 0 1 108 255
 0 1 133 255
 0 1 158 255
 0 1 183 255
 0 1 208 255
 0 1 233 255
 0 1 3 255
 0 1 28 255
 0 1 53 255
 0 1 78 255
 0 1 103 255
 0 1 128 255
 0 1 153 255
 0 1 178 255
 0 1 203 255
 0 1 229 255
 0 1 254 255
 0 1 23 255
 0 1 48 255
 0 1 73 255
 0 1 98 255
 0 1 122 255

As you can see, the seconds and minutes do not update. The seconds either has a 0 or a 1.

Additionally, if I have LSI enabled then I seem to lose systick

Any ideas as to what is going on and how to correct it?

Thanks.

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
February 8, 2023

After reading time, you have to read date, too.

JW

3 replies

shorai
shoraiAuthor
Associate III
February 8, 2023

Changing RCC_OscInitStruct.HSIState = RCC_LSI_OFF;

does not affect the result.

waclawek.jan
waclawek.janBest answer
Super User
February 8, 2023

After reading time, you have to read date, too.

JW

shorai
shoraiAuthor
Associate III
February 8, 2023

Thank you so much Jan, really appreciate, it works

I bookmarked the gotchas:-)

So annoying,

STM really need to offer a single GetDateTime and deprecate the getTime function