Skip to main content
monta
Associate III
July 20, 2015
Question

STM32F4 Disco Connect Under Reset

  • July 20, 2015
  • 2 replies
  • 671 views
Posted on July 20, 2015 at 21:54

Hi there , I had my STM32F407VG discovery board for a while now, till a few minutes earlier, I was trying to interface a button to PA13 ( I chose PA13 randomaly) to create a simple interaface for my project , but once I tired the button few times I did not work, What's even worse now my Discovery board is not detected by CooCox and on the ST Link Utility it says ''Cannot Connect to target , please Connect under Reset'' (which works).

How Can it revert it back to how it was ? Did I mess up anything ? Does PA13 have to do with anything of this ??

Thank you !!!
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    July 20, 2015
    Posted on July 20, 2015 at 22:53

    PA13 is SWDAT, it's part of the debug interface.

    Strap BOOT[0] High/VDD and erase the part with the ST-LINK Utilities. This will run the System Loader, instead of your code which immediate breaks the debugger's connection.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    monta
    montaAuthor
    Associate III
    July 20, 2015
    Posted on July 20, 2015 at 23:13

    Thank you !! as always you're the best !