Skip to main content
nikofionn
Associate
July 23, 2014
Question

[STM32F4 Disco] Connect CAN 1 RX to EXTI 0

  • July 23, 2014
  • 3 replies
  • 964 views
Posted on July 23, 2014 at 22:35

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    July 23, 2014
    Posted on July 23, 2014 at 22:40

    This forum software does not support posting from mobile devices (Phones, Tablets).

    Perhaps if it's connected to PD0?
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    nikofionn
    nikofionnAuthor
    Associate
    July 24, 2014
    Posted on July 24, 2014 at 10:32

    ****update****

    I just had a quick chat with an STM engineer, who told me, that what I am trying to do, will not work...

    There is no way to connect the interrupt behind the CAN filter to an EXTI line, because they are not working in STOP-Mode.

    So, there are two ways left to get a quick solution (without changing hardware):

    - Enter STOP-Mode via WFE - Wait for event. This would wake up the MCU without an ISR, which would be fine for now.

    - Enable the EXTI line connected to RX-Pin just before entering STOP-Mode and disabling the EXTI line again after wake up. Otherwise an Interrupt would occur with any CAN message, which is not my aim.

    I will try to get the STOP-Mode working using the WFE - sequence. Can anybody give me some hints? I will post my code later on ;)

    *********

    Good morning clive1,

    I reworked my posting, as I did not know, thath mobile devices are not supported :)

    Kind regards,

    Niko

    Tesla DeLorean
    Guru
    July 24, 2014
    Posted on July 24, 2014 at 16:18

    Your EXTI configuration is wrong

    // EXT_INT0 connect to Pin0 [GPIOD] = RX-PIN

    SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOD, GPIO_Pin_0);

    Should be

    // EXT_INT0 connect to Pin PD0

    SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOD, EXTI_PinSource0); 

    Whether the state of the pin is usable is debatable, not sure the if you want an Event, if you configured an Interrupt. I'd go for WFI
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..