Skip to main content
pa_it
Associate III
November 7, 2013
Question

STM32F4 DCMI no line interrupt

  • November 7, 2013
  • 1 reply
  • 805 views
Posted on November 07, 2013 at 21:06

Hi

I've some problems with the dcmi interface from my stm32f4 I've initialized the module for line and frame interrupts, but in debug I see only the frame complete interrupt, and a line count variable isn't incremented. Can anyone help me?

DCMI_DeInit();
DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMode_Continuous;
DCMI_InitStructure.DCMI_SynchroMode = DCMI_SynchroMode_Hardware;
DCMI_InitStructure.DCMI_PCKPolarity = DCMI_PCKPolarity_Falling;
DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_High;
DCMI_InitStructure.DCMI_HSPolarity = DCMI_HSPolarity_High;
DCMI_InitStructure.DCMI_CaptureRate = DCMI_CaptureRate_All_Frame;
DCMI_InitStructure.DCMI_ExtendedDataMode = DCMI_ExtendedDataMode_8b;
DCMI_Init(&DCMI_InitStructure);
/* DCMI Interrupts config ***************************************************/
DCMI_ITConfig(DCMI_IT_VSYNC, ENABLE);
DCMI_ITConfig(DCMI_IT_LINE, ENABLE);
DCMI_ITConfig(DCMI_IT_FRAME, ENABLE);
DCMI_ITConfig(DCMI_IT_ERR, ENABLE);
DCMI_ITConfig(DCMI_IT_OVF, ENABLE);
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);
NVIC_InitStructure.NVIC_IRQChannel = DCMI_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);

Best regards
    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    November 19, 2013
    Posted on November 19, 2013 at 11:39

    Hi Patrick,

    How is configured the IRQ handler?

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.