Skip to main content
azayetey
Associate
August 30, 2015
Question

STM32F4 corrupt memory/damaged MCU

Posted on August 30, 2015 at 16:53

Hello,

I've been working on a project on my STM32F4 Discovery for a few weeks now and it's been working fine. Today I connected a OV7670 camera and after uploading the code the discovery stopped working after a while for some reason. I removed all the wires that connect the camera but still it does not work.

I try to debug to see what is wrong but when I go into the SystemInit() function the debugger just hangs there and does not continue. The dissasembler just shows nothing after that. What is wrong? I tried a few times to erase the whole flash memory and reprogram but it did not help.

I'm using Coocox IDE and  STM32F407Discovery with stlink via usb
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    August 30, 2015
    Posted on August 30, 2015 at 17:29

    So do you actually STEP INTO SystemInit(), at what line of code explicitly does it stop? Is it waiting for a clock to start, a PLL to lock?

    Do you have another board to see if it's board/chip specific?

    Have you looked at the voltages on the board can checked if they are where they should be? ie VDD at 3.0V, VCAPs at 1.25V

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    dj_v14
    Associate II
    December 31, 2016
    Posted on December 31, 2016 at 10:57

    to_deletemr assioma

    ‌

    Hi,

    Around a year back you have faced this issue, and currently I am facing similar issue. Is it resolved? Can you please help me with the resolution?

    Thanks,

    Dhaval

    Tesla DeLorean
    Guru
    December 31, 2016
    Posted on December 31, 2016 at 17:26

    Please try not to reopen old threads where the OP hasn't even bothered to respond to the advice provided.

    If a part has been crashed by user code, strap BOOT0 high so it doesn't run and break the debugger interface. The system loader is in ROM/OTP it isn't something that is going to get randomly erased.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..