Question
STM32F4 bxCAN FiFo Release Issues
Posted on March 13, 2014 at 21:34
Can anyone tell me if the following is normal functionality of the RFR register:
Processor clock 168 MHz APB1 bus 42 MHz After reading the Receive FiFo and releasing by setting RFOM1 bit to 1 in the RF1R register, we must wait until the RFOM1 is reset to 0 by the hardware before exiting the interrupt. If we exit the interrupt while RFOM1 bit is still set, the interrupt routine is immediately re-entered and the subsequent reading of the RIR register returns a value with eroneous values. We never saw this issue using the an STM32F3 processor at 72 MHz and APB1 bus at 36 MHz. Thanks