Skip to main content
qinghai
Associate II
September 13, 2013
Question

stm32f4 adc dual model with dma

  • September 13, 2013
  • 3 replies
  • 966 views
Posted on September 13, 2013 at 17:54

hello everyone,

Now I use stm32f4 discovery. I want to use ADC example ''ADC_DualModeRegulSimu'' from the StdPeriph_Lib_V1.1.0 Project.

I have following questions:

1. They use ADC Dual Mode with DMA, but they don't active ADC_DMA(ADC1, enable);

2. In ADCx_CH10_CH11_Config() they selected 

  ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;

I don't know why is it? They used softwarestart of ADC, otherwise they don't active the trigger edge.

3. in DMA_Config() 

    DMA_InitStructure.DMA_Channel = DMA_Channel_0; 

  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&aADCDualConvertedValue;

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC_

CCR

_ADDRESS;

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

  DMA_InitStructure.DMA_BufferSize = 4;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_

HalfWord

;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_

HalfWord

;

I think ADC_CCR should be CDR.

 But in Dual Mode high 16 Bits of CDR save ADC2 data and low 16 Bits save ADC1 data. DMA_PeripheralDataSize should be defined as Word (32Bits) or I didn't really understand the data transfer between ADC_CDR and DMA_Memory. CDR send data of CH10 (ADC1), CH11(ADC2), CH11(ADC1), CH12(ADC2) in this example, the data in CDR has to be sent two times?

(CDR(15:0) then CDR(31:16)?).

Thank you very much for your attention and hope your answer!

#stm32f4-adc-dma
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
September 13, 2013
Posted on September 13, 2013 at 18:01

The DMA is enabled with

/* Enable DMA request after last transfer (Multi-ADC mode) */
ADC_MultiModeDMARequestAfterLastTransferCmd(ENABLE);

My example is about five posts in here

/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/ADC%20in%20Dual%20Mode%20Simultaneously&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=235

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
qinghai
qinghaiAuthor
Associate II
September 16, 2013
Posted on September 16, 2013 at 10:13

Thank you very much! From your code I knew how ADC dual mode works. 

qinghai
qinghaiAuthor
Associate II
September 17, 2013
Posted on September 17, 2013 at 11:03

Hello Clive1,

I run the code from you. It works very well. But I have also two questions:

1. in this program the dual mode with extern trigger is used. But in main function you used also ADC_SoftwareStartConv(ADC1)

is it necessary?

2. In datasheet of stm32f40xx writes  the maximal ADC Clock is 36 MHz. But in this case we have APB2CLK 84 MHz, use ADC_Prescaler_Div2, that means we use ADCCLK with 42 MHz. I see the example of MCD Application Team from standard peripherals library. They used also 42 MHz for the dual mode.

What is the really maximal ADC clock for the stm32f4?

Regards,