Skip to main content
borisw37
Visitor II
April 16, 2015
Question

STM32F4 8bit DMA to GPIO

  • April 16, 2015
  • 1 reply
  • 1111 views
Posted on April 16, 2015 at 17:05

Hello,

I'm relatively new to the STM32F4 family but have worked with other microcontrollers in the the past. I'm trying to use DMA to send 8bits of data at a time from a memory array to a GPIO (GPIO_C) using DMA with TIM4 as a trigger. I've played around with the DMA MEM to DAC example. What I'm confused by is: 1) Peripheral (GPIO_C) address. According to the datasheet GPIOC base addr = 0x40020800. GPIOx_ODR has offset of 0x So the peripheral address is0x40020814? 2) How do I DMA 8bits at a time to a 32bit GPIOC_ODR register? GPIOC_ODR is a 32 bit register with only the lower 16 being used. How do I write to lowest 8bits? Or bits 8..15? DMA Init has settings for chunk size.

DMA_InitStructure.DMA_PeripheralDataSize = DMA_MemoryDataSize_Byte;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

But how do I define which portion of the 32bit register will receive the 8bits? Thank you, Boris.
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 16, 2015
    Posted on April 16, 2015 at 17:27

    DMA_InitStructure.DMA_PeripheralDataSize = DMA_MemoryDataSize_Byte; // Peripheral Size!

    It's a small endian system writing at +0 gets bits 0..7, +1 8..15

    You could also use BSRR for dispersed bits.

    I believe I've posted several DMA to/from GPIO examples, with internal TIM, and external.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..