Skip to main content
bobot
Associate
November 18, 2012
Question

STM32F3DISCOVERY USB-Virtual Com Port?

  • November 18, 2012
  • 18 replies
  • 3621 views
Posted on November 18, 2012 at 14:16

Hi!

May I ask for help about setting up VCP with one?

I am currently looking over the files of STM32_USB-FS-Device_Lib_V3.4.0 (under virtual com port). I can't seem to understand how to tailor it with STM32F3Discovery. Or is it even possible to use it with STM32F3? Can anyone help me understand how to use the library with other USB capable STM32's? I am using IAR starter.

I am very new to STM32 MCUs. Just opened my STM32F3Discovery this week. I choose this board because of its included sensors. The objective simply to forward the readings of the sensor to a host PC. The data gathered will be used for academic purposes. So, for now, I wanted to connect it first with my PC through VCP.

Than you very much.

    This topic has been closed for replies.

    18 replies

    Tesla DeLorean
    Guru
    November 18, 2012
    Posted on November 18, 2012 at 15:52

    I'd probably start with the OTG library, and merge in the F3 firmware library.

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32_f105-07_f2_f4_usb-host-device_lib.zip

    And see if that works. Can't help you with IAR, could probably built a GNU or Keil project.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bobot
    bobotAuthor
    Associate
    November 19, 2012
    Posted on November 19, 2012 at 04:03

    @clive1

    Thank you sir... I have also looked into that library but I can't still figure out which of those source files are to be modified for stm32f3 (stm32F303). But I'll dig deeper...

    Kiel, would be fine for me... I just downloaded and installed one. I seems I like their IDE more. And since I am very new to this, I can basically pick and shift another IDE and/or toolchain.

    If it is not much to ask, can you make a sample project for me...?

    Thank you very much once again.
    Tesla DeLorean
    Guru
    November 19, 2012
    Posted on November 19, 2012 at 16:29

    Reviewing the code it looks to be closer to the older 3.4.0 track (now 4.0 mentioned in F3-Discovery firmware). Odd that ST doesn't have some examples, trying to merge something together, might take a day of two.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bobot
    bobotAuthor
    Associate
    November 26, 2012
    Posted on November 26, 2012 at 03:35

    Hi clive, 

    I wonder, that if you can still make that sample code... I am still in need of those. I mean, if you just have some time for it. thanks.

    The most concerning issue for me, actually, is the 'How tos' of the firmware usage. I wanted to know how do we pick those source/headers that we needed. It just seem to me that there is no documentation provided by ST. OR, I am just really that lost.  Some experienced 32-bitters users told me that firmwares provided by manufacturers for such MCUs are ''overwhelming'' for noobs. I may be that beginner! :)

    Nickname12657_O
    Associate III
    November 26, 2012
    Posted on November 26, 2012 at 15:15

    Hi Bobot,

    All the required for getting started with the STM32F3DISCOVERY is available throw

    http://www.st.com/internet/evalboard/product/254044.jsp?WT.ac=fp_sep12_stm32f3discovery

    . There is mainly the firmware package with various examples and the documentation describing how to use it.

    If you need the VCP driver, you can get it from

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/stm32_vcp.zip

    .

    I hope that this brings some help to you and I don't repeat things that you already know :).

    Cheers,

    STOne-32
    markmark9126
    Visitor II
    February 14, 2013
    Posted on February 14, 2013 at 17:01

    Hi Bobot,

    I have the same problem trying to figure out what bits of the source code I need to use. Have you been able to figure out how to get the virtual com port code working with the STM23F3discovery?
    Tesla DeLorean
    Guru
    February 14, 2013
    Posted on February 14, 2013 at 20:00

    V4 of the USB FS Device library has been released since this thread started. That has a virtual com port example. Haven't had cause to look it over yet.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    neels
    Visitor II
    February 23, 2013
    Posted on February 23, 2013 at 05:37

    Can you post the link to the v4 of USB FS library for STM32F37x devices ? 

    After the ST website has been upgraded to the new site, I am unable to find it. Also many of the application notes are now the older versions which don't have any mention of F3 in them and they appear under the STM32F3 microcontroller page. 

    Google cache has the newer versions of AN pdfs then the ST site. 

    Tesla DeLorean
    Guru
    February 23, 2013
    Posted on February 23, 2013 at 14:59

    Yeah, they seem to have made it impossibly difficult to find. I'll post the one I downloaded previously to my share.

    https://docs.google.com/file/d/0B7OY5pub_GfIN3EyMFlEZWhGMUk/edit?usp=sharing

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Amel NASRI
    ST Technical Moderator
    February 27, 2013
    Posted on February 27, 2013 at 14:48

    Also many of the application notes are now the older versions which don't have any mention of F3 in them and they appear under the STM32F3 microcontroller page.

     

    Which ones? May be they are the common ANs.

    Thanks,

    ST.MCU
    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.