Skip to main content
bmanogna
Visitor II
Jun 30, 2014 3:42 PM UTC
Question

STM32F373RC TTa output driving circuit

Posted on June 30, 2014 at 17:42

Hi all,

I would like to know where can i find the internal driving circuit schematics of a TTa output pin (PA0, pin 14) for the  STM32F373RC controller.

PS: I think i might be an open collector with an internal pull up resistor but cant be sure..

Thanks,

S.Bharath Manogna
    This topic has been closed for replies.

    2 replies

    chen
    Associate II
    Jun 30, 2014 4:20 PM UTC
    Posted on June 30, 2014 at 18:20

    Hi

    ''I would like to know where can i find the internal driving circuit schematics of a TTa output pin (PA0, pin 14) for the  STM32F373RC controller.''

    http://www.st.com/web/en/resource/technical/document/reference_manual/DM00041563.pdf

    Look in section 8 General-purpose I/Os (GPIO)

    ''PS: I think i might be an open collector with an internal pull up resistor but cant be sure..''

    Like most of the STM32 range, the output port is configurable : push/pull or open drain, with or with out pull up.

    Tesla DeLorean
    Guru
    Jun 30, 2014 4:27 PM UTC
    Posted on June 30, 2014 at 18:27

    The TTa pins are 3.3V tolerant, and connected to the ADC

    Whether they are Push-Pull or Open-Collector, or Pull-Up or Pull-Down, that's for YOU to configure.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..